Other Parts Discussed in Thread: DRA742, PMP, DRA752, SYSBIOS
Tool/software: Linux
Dear,
I faced the problem with 03_04 package.
I'm using "tda2xx_evm_linux_all" configuration for linux target.
The problem is that I can't enable the IPU1_0 CPU.
I just enabled the PROC_IPU1_0_INCLUDE as "yes" but below error happens.
[HOST] [IPU2 ] 89.096718 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 90.096748 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [DSP1 ] 89.780912 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 90.780943 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 90.052918 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 91.052949 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [IPU2 ] 91.096779 s: SYSTEM: Attaching to [IPU1-0] ...
I followed the flow in "VisionSDK_Linux_UserGuide.pdf" document and have never touched the source code even scripts except cfg.mk in apps/configs/tda2xx_evm_linux_all directory.
Thanks in advance.
BR.
Full logs are attached.
--------------------------------
U-Boot SPL 2016.05-00010-g9551b3d-dirty (Nov 16 2018 - 20:38:30)
DRA752-GP ES2.0
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
** First descriptor is NOT a primary desc on 1:1 **
Trying to boot from MMC1
reading dra7-ipu2-fw.lzop
spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
spl: error reading image dra7-ipu2-fw.lzop, err - -1
Error loading remotecore IPU2!,Continuing with boot ...
reading dra7-dsp1-fw.lzop
spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
spl: error reading image dra7-dsp1-fw.lzop, err - -1
Error loading remotecore DSP1!,Continuing with boot ...
reading dra7-dsp2-fw.lzop
spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
spl: error reading image dra7-dsp2-fw.lzop, err - -1
Error loading remotecore DSP2!,Continuing with boot ...
reading dra7-ipu1-fw.lzop
spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
spl: error reading image dra7-ipu1-fw.lzop, err - -1
Error loading remotecore IPU1!,Continuing with boot ...
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-00010-g9551b3d-dirty (Nov 16 2018 - 20:38:30 +0900)
Model: TI DRA742
Board: DRA74x EVM REV H.0
DRAM: 4 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
** First descriptor is NOT a primary desc on 1:1 **
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: eth0: ethernet@48484000
Hit any key to stop autoboot: 0
## Error: "board_findfdt" not defined
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
165 bytes read in 3 ms (53.7 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3559560 bytes read in 93 ms (36.5 MiB/s)
106875 bytes read in 15 ms (6.8 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x365088 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe2000, end 8ffff17a ... OK
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.84-00027-g018eb62-dirty (usnoh@usnoh-linux) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #3 SMP PREEMPT Fri Nov 16 20:51:00 KST 2018
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA742
[ 0.000000] Ignoring memory block 0x200000000 - 0x280000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x40300000, size 3 MiB
[ 0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x99000000, size 80 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x9e000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0xa1000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0xa3000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created DMA memory pool at 0xa9000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0xbe400000
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0xbfe00000 to fe600000 for dram barrier
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @ef631000 s14912 r8192 d21952 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 243520
[ 0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=PARTUUID=403a916e-02 rw rootwait ip=none mem=1024M
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 411860K/980992K available (6663K kernel code, 318K rwdata, 2392K rodata, 332K init, 286K bss, 364332K reserved, 204800K cma-reserved, 235520K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08e000c (9057 kB)
[ 0.000000] .init : 0xc08e1000 - 0xc0934000 ( 332 kB)
[ 0.000000] .data : 0xc0934000 - 0xc09839e0 ( 319 kB)
[ 0.000000] .bss : 0xc0985000 - 0xc09cc980 ( 287 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000004] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000016] Switching to timer-based delay loop, resolution 162ns
[ 0.000334] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000343] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000788] Console: colour dummy device 80x30
[ 0.000804] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000810] This ensures that you still see kernel messages. Please
[ 0.000816] update your kernel commandline.
[ 0.000829] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000842] pid_max: default: 32768 minimum: 301
[ 0.000935] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000947] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001491] Initializing cgroup subsys io
[ 0.001507] Initializing cgroup subsys memory
[ 0.001531] Initializing cgroup subsys devices
[ 0.001544] Initializing cgroup subsys freezer
[ 0.001554] Initializing cgroup subsys perf_event
[ 0.001565] Initializing cgroup subsys pids
[ 0.001592] CPU: Testing write buffer coherency: ok
[ 0.001797] /cpus/cpu@0 missing clock-frequency property
[ 0.001813] /cpus/cpu@1 missing clock-frequency property
[ 0.001823] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001863] Setting up static identity map for 0x80008340 - 0x800083a0
[ 0.080174] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080242] Brought up 2 CPUs
[ 0.080255] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.080261] CPU: All CPU(s) started in HYP mode.
[ 0.080267] CPU: Virtualization extensions available.
[ 0.081296] devtmpfs: initialized
[ 0.109844] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.110823] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.315821] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.315845] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.319838] pinctrl core: initialized pinctrl subsystem
[ 0.320740] NET: Registered protocol family 16
[ 0.321665] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.350242] cpuidle: using governor ladder
[ 0.380269] cpuidle: using governor menu
[ 0.388874] OMAP GPIO hardware version 0.1
[ 0.395444] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.411985] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 0.411998] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 0.421631] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.421641] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.422120] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.422130] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.422608] OMAP DMA hardware revision 0.0
[ 0.461618] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.462780] edma 43300000.edma: memcpy is disabled
[ 0.467518] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.471890] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.472064] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.472219] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.472373] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.472672] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.472861] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.475887] palmas 0-0058: IRQ missing: skipping irq request
[ 0.491301] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0
[ 0.563604] pcf857x 0-0020: probed
[ 0.564164] pcf857x 0-0021: probed
[ 0.564317] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.564715] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.564924] media: Linux media interface: v0.10
[ 0.564975] Linux video capture interface: v2.00
[ 0.565015] pps_core: LinuxPPS API ver. 1 registered
[ 0.565022] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.565050] PTP clock support registered
[ 0.565095] EDAC MC: Ver: 3.0.0
[ 0.565856] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.566144] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.566496] Advanced Linux Sound Architecture Driver Initialized.
[ 0.567352] clocksource: Switched to clocksource arch_sys_counter
[ 0.577896] NET: Registered protocol family 2
[ 0.578400] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.578462] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.578587] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.578635] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.578666] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.578867] NET: Registered protocol family 1
[ 0.579132] RPC: Registered named UNIX socket transport module.
[ 0.579141] RPC: Registered udp transport module.
[ 0.579148] RPC: Registered tcp transport module.
[ 0.579154] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.580172] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.589138] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.589771] NFS: Registering the id_resolver key type
[ 0.589806] Key type id_resolver registered
[ 0.589813] Key type id_legacy registered
[ 0.589881] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.591177] bounce: pool size: 64 pages
[ 0.591323] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.591336] io scheduler noop registered
[ 0.591347] io scheduler deadline registered
[ 0.591378] io scheduler cfq registered (default)
[ 0.596269] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.599502] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[ 0.599515] No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[ 0.599548] IO 0x20003000..0x20012fff -> 0x00000000
[ 0.599568] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 0.629714] dra7-pcie 51000000.pcie_rc: link is not up
[ 0.629890] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[ 0.629903] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.629913] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.629923] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.630329] PCI: bus0: Fast back to back transfers disabled
[ 0.630451] PCI: bus1: Fast back to back transfers enabled
[ 0.630533] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.630548] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.630560] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.630776] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.691565] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.694926] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[ 1.699169] console [ttyS0] enabled
[ 1.703560] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 302, base_baud = 3000000) is a 8250
[ 1.713256] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 303, base_baud = 3000000) is a 8250
[ 1.723321] [drm] Initialized drm 1.1.0 20060810
[ 1.728882] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.735524] [drm] No driver support for vblank timestamp query.
[ 1.741692] [drm] Initialized vdrm 1.0.0 20110917 on minor 0
[ 1.748879] OMAP DSS rev 6.1
[ 1.752619] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 1.768391] loop: module loaded
[ 1.771934] vmemexp device MAJOR num = 245
[ 1.776062] vmemexp class registered
[ 1.779793] /dev/vmemexp device registered
[ 1.783907] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[ 1.789620] nand: No NAND device found
[ 1.793391] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
[ 1.803326] m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)
[ 1.808744] 7 ofpart partitions found on MTD device spi32766.0
[ 1.814603] Creating 7 MTD partitions on "spi32766.0":
[ 1.819782] 0x000000000000-0x000000040000 : "QSPI.SPL"
[ 1.825916] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[ 1.832286] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[ 1.839214] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[ 1.845870] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[ 1.853264] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[ 1.859610] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[ 1.867363] libphy: Fixed MDIO Bus: probed
[ 1.917385] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.923508] davinci_mdio 48485000.mdio: detected phy mask fffffff3
[ 1.933967] libphy: 48485000.mdio: probed
[ 1.938041] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
[ 1.946082] davinci_mdio 48485000.mdio: phy[3]: device 48485000.mdio:03, driver unknown
[ 1.954793] cpsw 48484000.ethernet: Detected MACID = 7c:38:66:a1:e2:dc
[ 1.961491] cpsw 48484000.ethernet: cpts: overflow check period 800
[ 1.968509] cpsw 48484000.ethernet: cpsw: Detected MACID = 7c:38:66:a1:e2:dd
[ 1.977127] mousedev: PS/2 mouse device common for all mice
[ 1.983335] i2c /dev entries driver
[ 1.992098] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.997757] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 2.004144] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 2.010701] evm_3v3_sw: supplied by sysen1
[ 2.091132] mmc0: MAN_BKOPS_EN bit is not set
[ 2.103075] mmc0: new HS200 MMC card at address 0001
[ 2.118535] mmcblk0: mmc0:0001 MMC08G 7.25 GiB
[ 2.133326] mmcblk0boot0: mmc0:0001 MMC08G partition 1 8.00 MiB
[ 2.149556] mmcblk0boot1: mmc0:0001 MMC08G partition 2 8.00 MiB
[ 2.169213] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.180732] aic_dvdd: supplied by evm_3v3_sw
[ 2.186650] davinci-mcasp 4847c000.mcasp: invalid tdm slots: 0
[ 2.194321] NET: Registered protocol family 10
[ 2.200819] sit: IPv6 over IPv4 tunneling driver
[ 2.206003] NET: Registered protocol family 17
[ 2.210704] Key type dns_resolver registered
[ 2.215115] omap_voltage_late_init: Voltage driver support not added
[ 2.222016] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.228244] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.234940] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.241193] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.249459] Power Management for TI OMAP4+ devices.
[ 2.254519] Registering SWP/SWPB emulation handler
[ 2.260298] dmm 4e000000.dmm: workaround for errata i878 in use
[ 2.267517] dmm 4e000000.dmm: initialized all PAT entries
[ 2.274797] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.281474] [drm] No driver support for vblank timestamp query.
[ 2.287796] [drm] Initialized omapdrm 1.0.0 20110917 on minor 1
[ 2.294620] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.338698] asoc-simple-card sound0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
[ 2.358288] input: gpio_keys as /devices/platform/gpio_keys/input/input0
[ 2.365201] hctosys: unable to open rtc device (rtc0)
[ 2.378374] evm_1v8: disabling
[ 2.381454] aic_dvdd: disabling
[ 2.384614] vmmcwl_fixed: disabling
[ 2.388308] ldousb: disabling
[ 2.391702] ALSA device list:
[ 2.394679] #0: DRA7xx-EVM
[ 2.398237] Waiting for root device PARTUUID=403a916e-02...
[ 2.607382] mmc2: host does not support reading read-only switch, assuming write-enable
[ 2.622412] mmc2: new ultra high speed DDR50 SDHC card at address aaaa
[ 2.639416] mmcblk1: mmc2:aaaa SS08G 7.40 GiB
[ 2.649098] mmcblk1: p1 p2
[ 2.730983] EXT4-fs (mmcblk1p2): couldn't mount as ext3 due to feature incompatibilities
[ 2.742432] EXT4-fs (mmcblk1p2): couldn't mount as ext2 due to feature incompatibilities
[ 2.880252] EXT4-fs (mmcblk1p2): recovery complete
[ 2.885972] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.894149] VFS: Mounted root (ext4 filesystem) on device 179:50.
[ 2.900339] devtmpfs: mounted
[ 2.903504] Freeing unused kernel memory: 332K
[ 2.907983] This architecture does not have kernel memory protection.
[ 3.028620] systemd[1]: System time before build time, advancing clock.
[ 3.061001] random: systemd: uninitialized urandom read (16 bytes read, 19 bits of entropy available)
[ 3.073229] random: systemd: uninitialized urandom read (16 bytes read, 19 bits of entropy available)
[ 3.089652] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 3.108155] systemd[1]: Detected architecture arm.
[ 3.198514] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 3.208733] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 3.229165] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 3.253165] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 21 bits of entropy available)
[ 3.267692] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 21 bits of entropy available)
[ 3.329908] random: systemd: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[ 3.339445] random: systemd: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[ 3.349540] random: systemd: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[ 3.658813] systemd[1]: alignment.service: Found ordering cycle on alignment.service/start
[ 3.667129] systemd[1]: alignment.service: Found dependency on sysinit.target/start
[ 3.674868] systemd[1]: alignment.service: Found dependency on alignment.service/start
[ 3.682916] systemd[1]: alignment.service: Breaking ordering cycle by deleting job alignment.service/start
[ 3.692652] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with alignment.service/start
[ SKIP ] Ordering cycle found, skipping alignment.service
[ 3.729628] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 3.757634] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 3.787531] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.817630] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 3.852764] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 3.878180] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 3.907668] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 3.937688] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 3.967626] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 3.997525] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 4.018146] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 4.047515] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 4.078262] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.147550] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.189770] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 4.220010] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 4.277724] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 4.309732] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 4.328225] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ 4.343725] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 4.374600] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 4.385617] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 4.417603] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 4.437877] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 4.487821] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.507805] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 4.534296] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 4.557653] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 4.577782] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 4.597794] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[ OK ] Started Setup Virtual Console.
[ OK ] Started Remount Root and Kernel File Systems.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
Starting Apply Kernel Variables...
Starting udev Coldplug all Devices...
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 5.249821] systemd-journald[160]: Received request to flush runtime journal from PID 1
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Flush Journal to Persistent Storage.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
[ 5.649953] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
[ 5.673317] remoteproc0: 55020000.ipu is available
[ 5.678246] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 5.687243] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 5.698140] omap-rproc 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
[ 5.705966] remoteproc1: 40800000.dsp is available
[ 5.711942] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 5.722196] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 5.734413] omap-rproc 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
[ 5.745614] remoteproc2: 41000000.dsp is available
Starting Create Volatile Files and Directories...
[ 5.765874] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ OK ] Started udev Coldplug all Devices.[ 5.785844] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 5.978643] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ OK ] Started Create Volatile Files and Directories.
[ OK ] Found device /dev/ttyS0.
[ 6.084147] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc0
Starting Update UTMP about System Boot/Shutdown...
[ 6.161429] remoteproc1: registered virtio0 (type 7)
Starting Network Time Synchronization...
[ 6.200961] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ 6.346138] remoteproc0: registered virtio1 (type 7)
[ 6.423652] CAN device driver interface
[ 6.464483] SCSI subsystem initialized
[ 6.507576] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=358)
[ 6.651465] [drm] Initialized pvr 1.14.3699939 20110701 on minor 2
[ 6.679057] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 6.692816] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 6.701488] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ OK ] Started Network Time Synchronization.
[ 6.763309] remoteproc2: registered virtio2 (type 7)
Starting Synchronize System and HW clocks...
[ OK ] Reached target System Time Synchronized.
[ 6.863611] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 6.874476] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 6.884393] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ OK ] Started Synchronize System and HW clocks.
[ 6.908465] scsi host0: ahci
[ 6.911597] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 342
[ OK ] Reached target System Initialization.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started D-Bus System Message Bus.
[ 7.287433] ata1: SATA link down (SStatus 0 SControl 300)
Starting Network Service...
[ OK ] Started System Logging Service.
Starting Permit User Sessions...
[ 7.416556] net eth1: initializing cpsw version 1.15 (0)
Starting rc.pvr.service...
[ OK ] Started Daily Cleanup of Temporary Directories.[ 7.440857] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Reached target Timers.[ 7.472176] net eth0: ALE Table size 1024
[ 7.511023] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
Starting Login Service...
[ 7.522335] net eth0: initializing cpsw version 1.15 (0)
[ 7.550680] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ 7.567789] net eth0: phy found : id is : 0x20005c7a
[ OK ] Started Kernel Logging Service.
[ 7.580224] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
Starting Save/Restore Sound Card State...
[ OK ] Started Network Service.
[ OK ] Started Permit User Sessions.
[ OK ] Started rc.pvr.service.
[ OK ] Started Save/Restore Sound Card State.
[ 7.908073] remoteproc1: powering up 40800000.dsp
[ 7.945288] remoteproc1: Booting fw image dra7-dsp1-fw.xe66, size 6967543
[ 7.967963] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
[ 7.973855] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
[ 7.979801] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
[ 8.032503] remoteproc1: remote processor 40800000.dsp is now up
[ 8.046298] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 8.067811] remoteproc0: powering up 55020000.ipu
[ 8.095251] remoteproc0: Booting fw image dra7-ipu2-fw.xem4, size 9437412
[ 8.108178] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 8.178199] remoteproc0: remote processor 55020000.ipu is now up
[ 8.185646] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 8.198160] remoteproc2: powering up 41000000.dsp
[ 8.220783] remoteproc2: Booting fw image dra7-dsp2-fw.xe66, size 6967543
[ 8.244002] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
[ 8.249889] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
[ 8.255815] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
[ 8.305584] remoteproc2: remote processor 41000000.dsp is now up
[ 8.330991] virtio_rpmsg_bus virtio2: rpmsg host is online
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Reached target Sound Card.
Starting weston.service...
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS0.
[ 8.625380] usbcore: registered new interface driver usbfs
[ 8.631538] usbcore: registered new interface driver hub
[ 8.636958] usbcore: registered new device driver usb
[ OK ] Reached target Network.
Starting Network Name Resolution...
[ OK ] Started weston.service.
[ OK ] Started Login Service.
[ 8.712142] dwc3 48890000.usb: otg: primary host xhci-hcd.0.auto registered
[ 8.720539] dwc3 48890000.usb: otg: shared host xhci-hcd.0.auto registered
[ 8.729708] dwc3 48890000.usb: otg: can't start till gadget registers
[ 8.736302] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 8.745701] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 8.756564] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010
[ 8.765578] xhci-hcd xhci-hcd.1.auto: irq 500, io mem 0x488d0000
[ 8.773968] hub 1-0:1.0: USB hub found
[ 8.777862] hub 1-0:1.0: 1 port detected
[ 8.782148] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 8.787773] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 8.795613] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
Starting tiipclad-daemon.service...[ 8.806257] hub 2-0:1.0: USB hub found
Starting telnetd.service...
[ OK ] Started Network Name Resolution.
[ OK ] Started tiipclad-daemon.service.
[ OK ] Started telnetd.service.
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
root@dra7xx-evm:~# cd /opt/
ipks/ vision_sdk/
root@dra7xx-evm:~# cd /opt/vision_sdk/
root@dra7xx-evm:/opt/vision_sdk# ls
FragShader.fsh car.pod load_ocl_kos.sh setupUltrasonicPinMux.sh
FragShader3Dsfm.fsh cmemk.ko memcache_load.sh tda2exEnableAVB.sh
VertShader.vsh disableDssInterruptsOnA15.sh memcache_unload.sh ub964Init.sh
VertShader3Dsfm.vsh enableImx290.sh models vision_sdk_load.sh
VipClockInversion.sh enableIpu2CCSConectivity.sh opencl_env.sh vision_sdk_ov490_pinmux.sh
apps.out hdmiReceiverConfig.sh ov106x3Config.sh vision_sdk_unload.sh
bin jeep2.bmp pvrscope
root@dra7xx-evm:/opt/vision_sdk# ./load_ocl_kos.sh
[ 69.137101] allocated heap buffer 0x40400000 of size 0x100000
[ 69.143097] cmemk initialized
insmod: ERROR: could not load module /opt/vision_sdk/debugss_kmodule.ko: No such file or directory
insmod: ERROR: could not load module /opt/vision_sdk/gdbserverproxy.ko: No such file or directory
root@dra7xx-evm:/opt/vision_sdk# [ 69.793796] random: nonblocking pool is initialized
. vision_sdk_load.sh
[ 76.856481] DMA: Module install successful, device major num = 241
[ 76.862848] DRV: Module install successful
insmod: ERROR: could not load module ./bin/cmemk.ko: No such file or directory
./disableDssInterruptsOnA15.sh: line 11: @0x4A002AC4:: command not found
./disableDssInterruptsOnA15.sh: line 12: @0x4A002AC4:: command not found
./disableDssInterruptsOnA15.sh: line 13: @0x4A002AC4:: command not found
./disableDssInterruptsOnA15.sh: line 14: @0x4A002AC4:: command not found
./disableDssInterruptsOnA15.sh: line 15: @0x4A002AC4:: command not found
./disableDssInterruptsOnA15.sh: line 16: @0x4A002AC4:: command not found
./disableDssInterruptsOnA15.sh: line 17: @0x4A002AC4:: command not found
./disableDssInterruptsOnA15.sh: line 18: @0x4A002AC4:: command not found
./disableDssInterruptsOnA15.sh: line 19: @0x4A002AC4:: command not found
updated 0x4A002AC4 value is 00930000
root@dra7xx-evm:/opt/vision_sdk# . opencl_env.sh
root@dra7xx-evm:/opt/vision_sdk# ./apps.out
[HOST] OSA: MEM: 0: Mapped 0xa0100000 to 0xb69f1000 of size 0x00100000
[HOST] OSA: MEM: 1: Mapped 0x84203000 to 0xa6ff1000 of size 0x0fa00000
[HOST] OSA: MEM: 2: Mapped 0xa0200000 to 0xa6f31000 of size 0x00040000
[HOST] OSA: MEM: 3: Mapped 0xa02c0000 to 0xa6f71000 of size 0x00080000
[HOST] OSA: MEM: 4: Mapped 0x00000000 to 0x00000000 of size 0x00000000
[HOST] OSA: IPU1-0 Remote Log Shared Memory @ 0xa0200000
[HOST] OSA: HOST Remote Log Shared Memory @ 0xa024f140
[HOST] OSA: DSP1 Remote Log Shared Memory @ 0xa02769e0
[HOST] OSA: DSP2 Remote Log Shared Memory @ 0xa029e280
[HOST] OSA: EVE1 Remote Log Shared Memory @ 0xa02c5b20
[HOST] OSA: EVE2 Remote Log Shared Memory @ 0xa02ed3c0
[HOST] OSA: EVE3 Remote Log Shared Memory @ 0xa0314c60
[HOST] OSA: EVE4 Remote Log Shared Memory @ 0xa033c500
[HOST] OSA: IPU2 Remote Log Shared Memory @ 0xa0363da0
[HOST] [HOST ] 89.241109 s: SYSTEM: System A15 Init in progress !!!
[HOST] [DSP1 ] 14.777435 s: ***** DSP1 Firmware build time 21:06:05 Nov 16 2018
[HOST] [DSP1 ] 14.777496 s: *** SYSTEM: CPU Frequency <ORG = 600000000 Hz>, <NEW = 750000000 Hz>
[HOST] [DSP1 ] 14.777770 s: SYSTEM: System Common Init in progress !!!
[HOST] [DSP1 ] 14.778015 s: UTILS: CIO: Init Done !!!
[HOST] [DSP1 ] 14.778045 s: SYSTEM: IPC init in progress !!!
[HOST] [DSP1 ] 14.778045 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 15.778899 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 16.778930 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 17.778960 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 18.778991 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 19.779021 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 20.779052 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 21.779082 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 22.779113 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 23.779143 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 24.779143 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 25.779174 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 26.779204 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 27.779235 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 28.779265 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 29.779296 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 30.779326 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 31.779357 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 32.779387 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 33.779387 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 34.779418 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 35.779448 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 36.779479 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 37.779509 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 38.779540 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 39.779570 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 40.779601 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 41.779601 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 42.779631 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 43.779662 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 44.779692 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 45.779723 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 46.779753 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 47.779784 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 48.779814 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 49.779845 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 50.779845 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 51.779875 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 52.779906 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 53.779936 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 54.779967 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 55.779997 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 56.780028 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 57.780058 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 58.780089 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 59.780089 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 60.780119 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 61.780150 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 62.780180 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 63.780211 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 64.780241 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 65.780272 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 66.780302 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 67.780302 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 68.780333 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 69.780363 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 70.780394 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 71.780424 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 72.780455 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 73.780485 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 74.780516 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 75.780546 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 76.780546 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 77.780577 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 78.780607 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 79.780638 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 80.780668 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 81.780699 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 82.780729 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 83.780760 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 84.780790 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 85.780790 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 86.780821 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 87.780851 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 88.780882 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 15.050570 s: ***** DSP2 Firmware build time 21:06:03 Nov 16 2018
[HOST] [DSP2 ] 15.050661 s: *** SYSTEM: CPU Frequency <ORG = 600000000 Hz>, <NEW = 750000000 Hz>
[HOST] [DSP2 ] 15.050905 s: SYSTEM: System Common Init in progress !!!
[HOST] [DSP2 ] 15.051149 s: UTILS: CIO: Init Done !!!
[HOST] [DSP2 ] 15.051180 s: SYSTEM: IPC init in progress !!!
[HOST] [DSP2 ] 15.051210 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 16.050936 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 17.050936 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 18.050966 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 19.050997 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 20.051027 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 21.051058 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 22.051088 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 23.051119 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 24.051149 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 25.051149 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 26.051180 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 27.051210 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 28.051241 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 29.051271 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 30.051302 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 31.051332 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 32.051363 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 33.051393 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 34.051393 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 35.051424 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 36.051454 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 37.051485 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 38.051515 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 39.051546 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 40.051576 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 41.051607 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 42.051637 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 43.051637 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 44.051668 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 45.051698 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 46.051729 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 47.051759 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 48.051790 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 49.051820 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 50.051851 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 51.051851 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 52.051881 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 53.051912 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 54.051942 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 55.051973 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 56.052003 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 57.052034 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 58.052064 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 59.052095 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 60.052095 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 61.052125 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 62.052156 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 63.052186 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 64.052217 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 65.052247 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 66.052278 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 67.052308 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 68.052339 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 69.052339 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 70.052369 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 71.052400 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 72.052430 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 73.052461 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 74.052491 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 75.052522 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 76.052552 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 77.052583 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 78.052583 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 79.052613 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 80.052644 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 81.052674 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 82.052705 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 83.052735 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 84.052766 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 85.052796 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 86.052796 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 87.052827 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 88.052857 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 89.052888 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE1 ] 15.096138 s: ***** EVE Firmware build time 21:06:00 Nov 16 2018
[HOST] [EVE1 ] 15.097846 s: *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
[HOST] [EVE1 ] 15.100530 s: SYSTEM: System Common Init in progress !!!
[HOST] [EVE1 ] 15.102665 s: UTILS: CIO: Init Done !!!
[HOST] [EVE1 ] 15.103611 s: SYSTEM: IPC init in progress !!!
[HOST] [EVE1 ] 15.104587 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE1 ] 25.102086 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE1 ] 35.102330 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE1 ] 45.102604 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE1 ] 55.102879 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE1 ] 65.103153 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE1 ] 75.103428 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE1 ] 85.103702 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE2 ] 15.096596 s: ***** EVE Firmware build time 21:05:58 Nov 16 2018
[HOST] [EVE2 ] 15.098395 s: *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
[HOST] [EVE2 ] 15.101720 s: SYSTEM: System Common Init in progress !!!
[HOST] [EVE2 ] 15.103824 s: UTILS: CIO: Init Done !!!
[HOST] [EVE2 ] 15.104800 s: SYSTEM: IPC init in progress !!!
[HOST] [EVE2 ] 15.105776 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE2 ] 25.102086 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE2 ] 35.102330 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE2 ] 45.102604 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE2 ] 55.102879 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE2 ] 65.103153 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE2 ] 75.103428 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE2 ] 85.103702 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE3 ] 15.096382 s: ***** EVE Firmware build time 21:06:01 Nov 16 2018
[HOST] [EVE3 ] 15.098121 s: *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
[HOST] [EVE3 ] 15.100927 s: SYSTEM: System Common Init in progress !!!
[HOST] [EVE3 ] 15.103031 s: UTILS: CIO: Init Done !!!
[HOST] [EVE3 ] 15.103977 s: SYSTEM: IPC init in progress !!!
[HOST] [EVE3 ] 15.104922 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE3 ] 25.102055 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE3 ] 35.102330 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE3 ] 45.102604 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE3 ] 55.102879 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE3 ] 65.103153 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE3 ] 75.103428 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE3 ] 85.103702 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE4 ] 15.096596 s: ***** EVE Firmware build time 21:05:58 Nov 16 2018
[HOST] [EVE4 ] 15.098365 s: *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
[HOST] [EVE4 ] 15.101720 s: SYSTEM: System Common Init in progress !!!
[HOST] [EVE4 ] 15.103794 s: UTILS: CIO: Init Done !!!
[HOST] [EVE4 ] 15.104739 s: SYSTEM: IPC init in progress !!!
[HOST] [EVE4 ] 15.105746 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE4 ] 25.102055 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE4 ] 35.102330 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE4 ] 45.102604 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE4 ] 55.102879 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE4 ] 65.103153 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE4 ] 75.103428 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [EVE4 ] 85.103672 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [IPU2 ] 14.988074 s:
[HOST] [IPU2 ] EVE1 Image Load Completed
[HOST] [IPU2 ] 15.018575 s:
[HOST] [IPU2 ] EVE2 Image Load Completed
[HOST] [IPU2 ] 15.050051 s:
[HOST] [IPU2 ] EVE3 Image Load Completed
[HOST] [IPU2 ] 15.080674 s:
[HOST] [IPU2 ] EVE4 Image Load Completed
[HOST] [IPU2 ] 15.080796 s:
[HOST] [IPU2 ] EVE MMU configuration completed
[HOST] [IPU2 ] 15.080888 s:
[HOST] [IPU2 ] EVE MMU configuration completed
[HOST] [IPU2 ] 15.080949 s:
[HOST] [IPU2 ] EVE MMU configuration completed
[HOST] [IPU2 ] 15.081040 s:
[HOST] [IPU2 ] EVE MMU configuration completed
[HOST] [IPU2 ] 15.081101 s: ***** IPU2 Firmware build time 21:07:17 Nov 16 2018
[HOST] [IPU2 ] 15.081254 s: *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
[HOST] [IPU2 ] 15.084395 s: SYSTEM: System Common Init in progress !!!
[HOST] [IPU2 ] 15.095193 s: UTILS: CIO: Init Done !!!
[HOST] [IPU2 ] 15.095345 s: SYSTEM: IPC init in progress !!!
[HOST] [IPU2 ] 15.095437 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 16.094735 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 17.094766 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 18.094796 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 19.094827 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 20.094857 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 21.094888 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 22.094918 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 23.094949 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 24.094949 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 25.094979 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 26.095010 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 27.095040 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 28.095071 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 29.095101 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 30.095132 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 31.095162 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 32.095162 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 33.095193 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 34.095223 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 35.095254 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 36.095284 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 37.095315 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 38.095345 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 39.095376 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 40.095376 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 41.095406 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 42.095437 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 43.095467 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 44.095498 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 45.095528 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 46.095559 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 47.095589 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 48.095620 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 49.095620 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 50.095650 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 51.095681 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 52.095711 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 53.095742 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 54.095772 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 55.095803 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 56.095833 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 57.095864 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 58.095864 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 59.095894 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 60.095925 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 61.095955 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 62.095986 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 63.096016 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 64.096047 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 65.096077 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 66.096108 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 67.096108 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 68.096138 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 69.096169 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 70.096199 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 71.096230 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 72.096260 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 73.096291 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 74.096321 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 75.096321 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 76.096352 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 77.096382 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 78.096413 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 79.096443 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 80.096474 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 81.096504 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 82.096535 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 83.096565 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 84.096565 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 85.096596 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 86.096626 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 87.096657 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 88.096687 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 89.096718 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [IPU2 ] 90.096748 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [DSP1 ] 89.780912 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP1 ] 90.780943 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 90.052918 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 91.052949 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [IPU2 ] 91.096779 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [DSP1 ] 91.780973 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 92.052979 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [IPU2 ] 92.096779 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [DSP1 ] 92.781004 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 93.053010 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [IPU2 ] 93.096809 s: SYSTEM: Attaching to [IPU1-0] ...
[HOST] [DSP1 ] 93.781034 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [DSP2 ] 94.053040 s: SYSTEM: Attaching to [IPU2] ...
[HOST] [IPU2 ] 94.096840 s: SYSTEM: Attaching to [IPU1-0] ...
^C
root@dra7xx-evm:/opt/vision_sdk# [ 260.037386] omap-mailbox 48840000.mailbox: Try increasing MBOX_TX_QUEUE_LEN
[ 260.044387] omap-rproc 40800000.dsp: PM mbox_send_message failed: -105
[ 261.037380] omap-mailbox 48842000.mailbox: Try increasing MBOX_TX_QUEUE_LEN
[ 261.044376] omap-rproc 41000000.dsp: PM mbox_send_message failed: -105