Tool/software: Code Composer Studio
Hi there,
I need to debug what happen at boot time.
I'm using CCS5.5, TMS320C6418 target and developing a custom board.
I need to see the content of the onchip RAM at address 0x00 right after reset and before code located at address 0 is exetued (i.e. I need to see if ROM boot mode is correctly working copying the first 1k of bytes from the external memory into the onchip ram).
How can I debug this with the emulator so that I can be sure that I see what actually happen at boot time?
Thank you
Regards