Hello, TI Experts,
Our customer sent us questions about USB of AM5728.
They would like to use usb1_xx pins for USB2.0 and USB3.0.
Question:
1: usb1_xx pins automatically changed from USB3.0 to USB2.0, if USB3.0 connection fails.
Is this understanding correct?
2: Could you tell us USB2.0 and USB3.0 initialize sequence?
- Initialize sequence is "USB2.0 -> USB3.0" or
- Initialize sequence is "USB3.0 -> USB2.0" or
- Both USB2.0 and USB3.0 are initialized at the same time.
Which is correct?
Best regards,