Hi,
Some moths ago I posted this problem related to TMS320C6748:
As we told you, we found a short in some pins of the JTAG connector and we had to buy a new one. We have been working with the new board with no problems whatsoever until yesterday. Similarly to the post I have referred to, without apparent reason it stopped working showing the same error:
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 7.0.48.0)
We checked the same affected pins of the JTAG connector and we found no short in this case. We tried with a different debug probe but the problem persists. Also, we have followed all the steps you suggested in the previous post with no result.
Additionally, we have tried to load the .bin in the Flash memory and run the program without the debug probe and it works normally, so the problem seems to be only related to the JTAG interface.
Since it is the second board we have this problem with, we would want to know if there is a potential reason to be causing this failure. Do you have any idea about what could be happening?
Best regards,
Juan