Other Parts Discussed in Thread: BEAGLEBOARD-X15, , DRA752, TMP102, DRA742, TPS51200, TPD12S015, TLV320AIC3104
Tool/software: Linux
Hello everyone,
I am using BeagleBone Black X15 dev board and processor SDK 5 with default device tree and kernel settings.
When I tried to assign xref_clk1 (or any other xref_clk) to ahclkx, Linux doesn't boot anymore (kernel panic).
Here is the device tree snippet for mcasp2 configuration:
&mcasp2 {
#sound-dai-cells = <0>;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&mcasp2_pins_default>;
assigned-clocks = <&mcasp2_ahclkx_mux>;
assigned-clock-parents = <&ref_clkin1_ck>;
op-mode = <0>; /* MCASP_IIS_MODE */
tdm-slots = <2>;
/* mcasp1_axr0 = RX, mcasp1_axr1 = TX */
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */
2 1 0 0 // AXR0 and AXR1 pins
0 0 0 0
0 0 0 0
0 0 0 0
>;
tx-num-evt = <32>;
rx-num-evt = <32>;
};
Pin muxing is correct also (E17 ball is set to xref_clk1 mode).
What could be the problem here? When I select abe_24m_fclk instead of any xrefs, Linux boots and mcasp works fine.