Tool/software: Linux
Hello,
To recap, I am trying to implement the following scenario on TDA2x EVM:
(1) Transfer 4 test images from PC to EVM
(2) Run OpenGL-based SRV algorithm on the 4 images using on-board SGX GPU
(3) Transfer SRV output image from EVM to PC
What is TI's recommended development environment to implement this scenario:
- OS - Windows or Linux?
-
- I am asking this question because, as I understand it, OpenGL-ES API is supported on both Windows and Linux, and build process is essentially cross-compilation for target. So conceptually, as long as the relevant OpenGL-ES library is present on the PC, one could build the application on either OS. However, in some E2E forum posts, TI experts have pointed to the kmscube and similar applications, which appear to run exclusively on the Linux OS.
2. Build system - CCS or Makefile-based?
-
- As I understand it, even CCS uses the Make system internally. But I remember reading on some E2E forum post(s) that TDA2x Linux-based development should be carried out using pure Makefile-based approach. So it would be nice if TI can clarify this point.
PS: I am still going through the Vision SDK documentation and reference use-cases, but I would really appreciate it if TI experts can fill in the blanks and help me leap ahead.
Thank you.