Hi,
I am doing sparse training after stage L1 on caffe-jacinto.
I checked the solver_train.prototxt in trained model. There are some parameters for sparse training but I don't get the meaning of them. Those parameters are showed below:
display_sparsity: 2000
sparse_mode: SPARSE_UPDATE
sparsity_target: 0.7
sparsity_step_factor: 0.05
sparsity_step_iter: 2000
sparsity_start_iter: 0
sparsity_start_factor: 0.25
sparsity_threshold_maxratio: 0.2
sparsity_itr_increment_bfr_applying: true
sparsity_threshold_value_max: 0.2
I can understand display_sparsity, sparsity_target, but I'm confused about the others.
Can you describe how to use sparse training parameters in solver.prototxt ?
Is there any description or tips on parameters of sparse training ?