DRA624 SPI0 interface works in master mode , Can SPI0 interface work with three loads?(at a maximum of 25pF) at the maximum speed of 48MHZ? What's the problem?thank you very much!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DRA624 SPI0 interface works in master mode , Can SPI0 interface work with three loads?(at a maximum of 25pF) at the maximum speed of 48MHZ? What's the problem?thank you very much!
Hey user,
The SPI0 interface timings will be roughly equivalent to the datasheet values for SPI2 and SPI3 with a larger load (max 24 MHz). If you wanted to be more precise, you could simulate your particular PCB topology using IBIS models.
Regards,
Kyle