Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Tool/software: Linux
I have been struggling to get my OMAP-L138 to boot the Linux SDK v5.3 over NFS using TFTP. Nothing I have tried has worked. Has anyone else been successful using TFTP with an OMAP-L138 LCDK?
I was able to load the pre-built binary files onto an SD card.
When I configure the SDK for bootup from the SD card, it works.
I can log in as root.
I can connect to the instance of matrix using a web browser.
I will attach four Libre Office documents with notes:
- workstation_setup.odt
- boot_sdk_from_sdcard.odt
- boot_sdk_over_nfs-first_attempt-FAILED.odt
- boot_sdk_over_nfs-second_attempt-FAILED.odt
I am not an expert in Linux.
I am not an expert in uboot.
I figure I am missing something that someone experienced with Linux and uboot will spot and set me straight.
Thanks in advance for any guidance.
workstation_setup.docxboot_sdk_from_sdcard.docxboot_sdk_over_nfs-first_attempt-FAILED.docxboot_sdk_over_nfs-second_attempt-FAILED.docx