Part Number: TMDX654GPEVM
Tool/software: Linux
I am following the Matrix User's Guide:
I power up the EVM with the out-of-the-box SD Card without the display module connected. I want to use the remote matrix option instead. The ipconfig command is not found so I use "ip address":
root@am65xx-evm:~# ip address
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
inet 127.0.0.1/8 scope host lo
valid_lft forever preferred_lft forever
inet6 ::1/128 scope host
valid_lft forever preferred_lft forever
2: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
link/ether f4:84:4c:ed:38:8d brd ff:ff:ff:ff:ff:ff
inet6 fe80::f684:4cff:feed:388d/64 scope link
valid_lft forever preferred_lft forever
3: eth1: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc fq_codel state DOWN group default qlen 1000
link/ether 8e:10:86:74:8b:a3 brd ff:ff:ff:ff:ff:ff
4: eth2: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc fq_codel state DOWN group default qlen 1000
link/ether fa:67:b5:40:c6:bc brd ff:ff:ff:ff:ff:ff
eth0 does not have an IPV4 address. So I tried to connect Ethernet cable and enter inet6: http://[fe80::f684:4cff:feed:388d]:80 to the address bar. The browser prompted:
This page isn't working. [fe80::f684:4cff:feed:388d] did not send any data. ERR_EMPTY_RESPONSE.
How do I get the out-of-the-box SD Card boot to work with the URL using Remote Matrix?
Thanks.