Tool/software: TI-RTOS
Hello,
We expirience rare problems with both PRP mode via PRU-ICSS and PRU_EMAC when PRU stops transferring packets for short period of time. I managed to identify that it caused by PRU by taking PRP statistics. Currently it happens on PRU-ICSS-HSR-PRP-DAN_01.00.03.02 package but I do not hope it is fixed in PRU-ICSS-HSR-PRP-DAN_01.00.04.02, though I will try to migrate my code.
The time is around 32.5ms.
We send packets with constant rate (sampled valued data) and this problem sometimes happens once per 10 seconds, sometimes once per half hour. But the the pause in RX (32.5ms) is more or less constant.
For me it looks like internal watchdog reboot of PRU or kind of DDoS protection, but I'm not sure and have no idea of how to proof that theory.
I'm now trying to migrate to 01.00.04.02 to check if fixed already, but I'd like to hear if it is known issue and if this time means something to TI developers.
Thanks, Alexander.