Tool/software: Linux
How to use hardware to decode H264 on J6 platform? Do you have relevant libraries and documents? Linux 3.14.49 is currently in use
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
How to use hardware to decode H264 on J6 platform? Do you have relevant libraries and documents? Linux 3.14.49 is currently in use
sdk :ti-glsdk_dra7xx-evm_7_02_00_02
Hi Guangyu li,
You can run viddec3test to decode and display h264/mpeg4 and mpeg2 streams. To invoke IVAHD from A15, DCE APIs are used.
Refer this link in GLSDK userguide
Refer omapdrmtest repository for the source code
http://git.ti.com/glsdk/omapdrmtest
You can use gstreamer also to decode and display h264 stream.
Thanks
Ramprasad
Hi Ramprasad
The SDK has to be installed on Ubuntu 14.04 operating system?
Can it be used on 16.04?
Hi Guangyu li,
Last SDK made on Linux 3.14 kernel is v7.04
downloads.ti.com/.../index_FDS.html
The Software developer guide says it works on Ubuntu 12.04 only. But installation on 14.04 should not be a problem.
Do you see any issues ?
Thanks
Ramprasad
Hi Ramprasad
Failure to create Building Yocto Filesystem
./bin/setup-yocto.sh
[PSDKLA]>
[PSDKLA]> Testing for yocto-layers
[PSDKLA]> ERROR: yocto-layers is not present
[PSDKLA]> Please run setup.sh and answer 'yes' to fetch-sources prompt
[PSDKLA]> Refer to the Processor SDK Linux Automotive Software Developers Guide for details
[PSDKLA]> Exiting...
Software version:
1. ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01
2. gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf
3. CCS6.2.0.00050_linux-x64
Hi Guangu li,
Did you install the SDK from this installer ti-processor-sdk-linux-automotive-dra7xx-evm-5.00.00.01-installer.bin downloaded from http://downloads.ti.com/infotainment/esd/jacinto6/processor-sdk-linux-automotive/5_00_00_01/index_FDS.html
After installation, the main SDK installer directory should have a directory yocto-layers.
Please refer the Software developer guide
and
Thanks
Ramprasad
Hi Ramprasad
Is the yocto-layers file created by installing SDK Linux Automotive?
When I install SDK here, I only have the following files
bin example-applications Makefile uninstall
board-support filesystem Rules.make uninstall.dat
component-sources gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf.tar.xz setup.sh Uninstall Processor SDK Linux Automotive.desktop
docs gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf.tar.xz test-bench
etc linux-devkit ti-devkit
Hi gangyu li,
I reinstalled SDK5.01 installer and checked. Yes, installer doesn't create the yocto-layers directory.
You need to execute bin/fetch-sources.sh script once to get this directory.
Thanks
Ramprasad
Hi Ramprasad
Wget environment issues cause update failures
Please confirm it
https_proxy = http://socks.example.com:1080
http_proxy = http://socks.example.com:1080
ftp_proxy = http://socks.example.com:1080
no_proxy = example.com:1080;127.0.0.1
use_proxy = on
Hi Gangyu li,
did you refer this link?
https://wiki.yoctoproject.org/wiki/Working_Behind_a_Network_Proxy
Thanks
Ram
Hi Ramprasad
Building Yocto Filesystem Error Please Help Solve
/* * DO NOT EDIT THIS FILE BY HAND! * It is generated by /home/yongjin/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/base/MKlib_gen.sh generated. * * This is a file of trivial functions generated from macro * definitions in curses.h to satisfy the XSI Curses requirement * that every macro also exist as a callable function. * * It will never be linked unless you call one of the entry * points with its normal macro definition disabled. In that * case, if you have no shared libraries, it will indirectly * pull most of the rest of the library into your link image. */ #define NCURSES_ATTR_T int #include <ncurses_cfg.h> #undef NCURSES_NOMACROS /* _this_ file uses macros */ #include <curses.priv.h> #undef vw_scanw #undef vwscanw #undef vw_printw #undef vwprintw NCURSES_EXPORT(int) (addch) (const chtype z) { T((T_CALLED("addch(%s)"), _tracechtype2(0,z))); returnCode(waddch(stdscr,z)); } NCURSES_EXPORT(int) (addchnstr) (const chtype * a1, int z) { T((T_CALLED("addchnstr(%p,%d)"), (const void *)a1, z)); returnCode(waddchnstr(stdscr,a1,z)); } NCURSES_EXPORT(int) (addchstr) (const chtype * z) { T((T_CALLED("addchstr(%p)"), (const void *)z)); returnCode(waddchnstr(stdscr,z,-1)); } NCURSES_EXPORT(int) (addnstr) (const char * a1, int z) { T((T_CALLED("addnstr(%s,%d)"), _nc_visbuf2(0,a1), z)); returnCode(waddnstr(stdscr,a1,z)); } NCURSES_EXPORT(int) (addstr) (const char * z) { T((T_CALLED("addstr(%s)"), _nc_visbuf2(0,z))); returnCode(waddnstr(stdscr,z,-1)); } NCURSES_EXPORT(int) (attroff) (int z) { T((T_CALLED("attroff(%s)"), _traceattr2(0,(chtype)z))); returnCode(wattr_off(stdscr, (attr_t)(z), # 39 "_22677.c" 3 4 ((void *)0) # 39 "_22677.c" )); } NCURSES_EXPORT(int) (attron) (int z) { T((T_CALLED("attron(%s)"), _traceattr2(0,(chtype)z))); returnCode(wattr_on(stdscr, (attr_t)(z), # 45 "_22677.c" 3 4 ((void *)0) # 45 "_22677.c" )); } NCURSES_EXPORT(int) (attrset) (int z) { T((T_CALLED("attrset(%s)"), _traceattr2(0,(chtype)z))); returnIntAttr((attr_t)((stdscr) ? ((stdscr)->_attrs = (attr_t)(z), (0)) : (-1))); } NCURSES_EXPORT(int) (attr_get) (attr_t * a1, short * a2, void * z) { T((T_CALLED("attr_get(%p,%p,%p)"), (const void *)a1, (const void *)a2, (const void *)z)); returnCode(((void)((a1) != (void *)0 && (*(a1) = (stdscr)->_attrs)), (void)((a2) != (void *)0 && (*(a2) = (short)((int)((((unsigned long)((stdscr)->_attrs) & ((((1UL) << 8) - 1UL) << ((0) + 8))) >> 8))))), (0))); } NCURSES_EXPORT(int) (attr_off) (attr_t a1, void * z) { T((T_CALLED("attr_off(%s,%p)"), _traceattr2(0,a1), (const void *)z)); returnCode(wattr_off(stdscr,a1,z)); } NCURSES_EXPORT(int) (attr_on) (attr_t a1, void * z) { T((T_CALLED("attr_on(%s,%p)"), _traceattr2(0,a1), (const void *)z)); returnCode(wattr_on(stdscr,a1,z)); } NCURSES_EXPORT(int) (attr_set) (attr_t a1, short a2, void * z) { T((T_CALLED("attr_set(%s,%d,%p)"), _traceattr2(0,a1), a2, (const void *)z)); returnCode(((stdscr)->_attrs = (((a1) & ~((((1UL) << 8) - 1UL) << ((0) + 8))) | (attr_t)((a2) << ((0) + 8))), (0))); } NCURSES_EXPORT(int) (bkgd) (chtype z) { T((T_CALLED("bkgd(%s)"), _tracechtype2(0,z))); returnCode(wbkgd(stdscr,z)); } NCURSES_EXPORT(void) (bkgdset) (chtype z) { T((T_CALLED("bkgdset(%s)"), _tracechtype2(0,z))); wbkgdset(stdscr,z); returnVoid; } NCURSES_EXPORT(int) (border) (chtype a1, chtype a2, chtype a3, chtype a4, chtype a5, chtype a6, chtype a7, chtype z) { T((T_CALLED("border(%s,%s,%s,%s,%s,%s,%s,%s)"), _tracechtype2(0,a1), _tracechtype2(1,a2), _tracechtype2(2,a3), _tracechtype2(3,a4), _tracechtype2(4,a5), _tracechtype2(5,a6), _tracechtype2(6,a7), _tracechtype2(7,z))); returnCode(wborder(stdscr, a1, a2, a3, a4, a5, a6, a7, z)); } NCURSES_EXPORT(int) (box) (WINDOW * a1, chtype a2, chtype z) { T((T_CALLED("box(%p,%s,%s)"), (const void *)a1, _tracechtype2(1,a2), _tracechtype2(2,z))); returnCode(wborder(a1, a2, a2, z, z, 0, 0, 0, 0)); } NCURSES_EXPORT(int) (chgat) (int a1, attr_t a2, short a3, const void * z) { T((T_CALLED("chgat(%d,%s,%d,%p)"), a1, _traceattr2(1,a2), a3, (const void *)z)); returnCode(wchgat(stdscr,a1,a2,a3,z)); } NCURSES_EXPORT(int) (clear) (void) { T((T_CALLED("clear()"))); returnCode(wclear(stdscr)); } NCURSES_EXPORT(int) (clrtobot) (void) { T((T_CALLED("clrtobot()"))); returnCode(wclrtobot(stdscr)); } NCURSES_EXPORT(int) (clrtoeol) (void) { T((T_CALLED("clrtoeol()"))); returnCode(wclrtoeol(stdscr)); } NCURSES_EXPORT(int) (color_set) (short a1, void * z) { T((T_CALLED("color_set(%d,%p)"), a1, (const void *)z)); returnCode(wcolor_set(stdscr,a1,z)); } NCURSES_EXPORT(int) (COLOR_PAIR) (int z) { T((T_CALLED("COLOR_PAIR(%d)"), z)); returnCode(((z) << ((0) + 8))); } NCURSES_EXPORT(int) (delch) (void) { T((T_CALLED("delch()"))); returnCode(wdelch(stdscr)); } NCURSES_EXPORT(int) (deleteln) (void) { T((T_CALLED("deleteln()"))); returnCode(winsdelln(stdscr,-1)); } NCURSES_EXPORT(int) (echochar) (const chtype z) { T((T_CALLED("echochar(%s)"), _tracechtype2(0,z))); returnCode(wechochar(stdscr,z)); } NCURSES_EXPORT(int) (erase) (void) { T((T_CALLED("erase()"))); returnCode(werase(stdscr)); } NCURSES_EXPORT(chtype) (getbkgd) (WINDOW * z) { T((T_CALLED("getbkgd(%p)"), (const void *)z)); returnChtype(((z)->_bkgd)); } NCURSES_EXPORT(int) (getch) (void) { T((T_CALLED("getch()"))); returnCode(wgetch(stdscr)); } NCURSES_EXPORT(int) (getnstr) (char * a1, int z) { T((T_CALLED("getnstr(%s,%d)"), _nc_visbuf2(0,a1), z)); returnCode(wgetnstr(stdscr, a1, z)); } NCURSES_EXPORT(int) (getstr) (char * z) { T((T_CALLED("getstr(%s)"), _nc_visbuf2(0,z))); returnCode(wgetnstr(stdscr, z, -1)); } NCURSES_EXPORT(int) (hline) (chtype a1, int z) { T((T_CALLED("hline(%s,%d)"), _tracechtype2(0,a1), z)); returnCode(whline(stdscr, a1, z)); } NCURSES_EXPORT(chtype) (inch) (void) { T((T_CALLED("inch()"))); returnChtype(winch(stdscr)); } NCURSES_EXPORT(int) (inchnstr) (chtype * a1, int z) { T((T_CALLED("inchnstr(%p,%d)"), (const void *)a1, z)); returnCode(winchnstr(stdscr,a1,z)); } NCURSES_EXPORT(int) (inchstr) (chtype * z) { T((T_CALLED("inchstr(%p)"), (const void *)z)); returnCode(winchnstr(stdscr, z, -1)); } NCURSES_EXPORT(int) (innstr) (char * a1, int z) { return winnstr(stdscr,a1,z) ; } NCURSES_EXPORT(int) (insch) (chtype z) { T((T_CALLED("insch(%s)"), _tracechtype2(0,z))); returnCode(winsch(stdscr,z)); } NCURSES_EXPORT(int) (insdelln) (int z) { T((T_CALLED("insdelln(%d)"), z)); returnCode(winsdelln(stdscr,z)); } NCURSES_EXPORT(int) (insertln) (void) { T((T_CALLED("insertln()"))); returnCode(winsdelln(stdscr,1)); } NCURSES_EXPORT(int) (insnstr) (const char * a1, int z) { T((T_CALLED("insnstr(%s,%d)"), _nc_visbuf2(0,a1), z)); returnCode(winsnstr(stdscr,a1,z)); } NCURSES_EXPORT(int) (insstr) (const char * z) { T((T_CALLED("insstr(%s)"), _nc_visbuf2(0,z))); returnCode(winsnstr(stdscr, z, -1)); } NCURSES_EXPORT(int) (instr) (char * z) { T((T_CALLED("instr(%s)"), _nc_visbuf2(0,z))); returnCode(winnstr(stdscr, z, -1)); } NCURSES_EXPORT(int) (move) (int a1, int z) { T((T_CALLED("move(%d,%d)"), a1, z)); returnCode(wmove(stdscr,a1,z)); } NCURSES_EXPORT(int) (mvaddch) (int a1, int a2, const chtype z) { T((T_CALLED("mvaddch(%d,%d,%s)"), a1, a2, _tracechtype2(2,z))); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : waddch(stdscr,z))); } NCURSES_EXPORT(int) (mvaddchnstr) (int a1, int a2, const chtype * a3, int z) { T((T_CALLED("mvaddchnstr(%d,%d,%p,%d)"), a1, a2, (const void *)a3, z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : waddchnstr(stdscr,a3,z))); } NCURSES_EXPORT(int) (mvaddchstr) (int a1, int a2, const chtype * z) { T((T_CALLED("mvaddchstr(%d,%d,%p)"), a1, a2, (const void *)z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : waddchnstr(stdscr,z,-1))); } NCURSES_EXPORT(int) (mvaddnstr) (int a1, int a2, const char * a3, int z) { T((T_CALLED("mvaddnstr(%d,%d,%s,%d)"), a1, a2, _nc_visbuf2(2,a3), z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : waddnstr(stdscr,a3,z))); } NCURSES_EXPORT(int) (mvaddstr) (int a1, int a2, const char * z) { T((T_CALLED("mvaddstr(%d,%d,%s)"), a1, a2, _nc_visbuf2(2,z))); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : waddnstr(stdscr,z,-1))); } NCURSES_EXPORT(int) (mvchgat) (int a1, int a2, int a3, attr_t a4, short a5, const void * z) { T((T_CALLED("mvchgat(%d,%d,%d,%s,%d,%p)"), a1, a2, a3, _traceattr2(3,a4), a5, (const void *)z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : wchgat(stdscr,a3,a4,a5,z))); } NCURSES_EXPORT(int) (mvdelch) (int a1, int z) { T((T_CALLED("mvdelch(%d,%d)"), a1, z)); returnCode((wmove(stdscr,a1,z) == (-1) ? (-1) : wdelch(stdscr))); } NCURSES_EXPORT(int) (mvgetch) (int a1, int z) { T((T_CALLED("mvgetch(%d,%d)"), a1, z)); returnCode((wmove(stdscr,a1,z) == (-1) ? (-1) : wgetch(stdscr))); } NCURSES_EXPORT(int) (mvgetnstr) (int a1, int a2, char * a3, int z) { T((T_CALLED("mvgetnstr(%d,%d,%s,%d)"), a1, a2, _nc_visbuf2(2,a3), z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : wgetnstr(stdscr,a3,z))); } NCURSES_EXPORT(int) (mvgetstr) (int a1, int a2, char * z) { T((T_CALLED("mvgetstr(%d,%d,%s)"), a1, a2, _nc_visbuf2(2,z))); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : wgetnstr(stdscr, z, -1))); } NCURSES_EXPORT(int) (mvhline) (int a1, int a2, chtype a3, int z) { T((T_CALLED("mvhline(%d,%d,%s,%d)"), a1, a2, _tracechtype2(2,a3), z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : whline(stdscr,a3,z))); } NCURSES_EXPORT(chtype) (mvinch) (int a1, int z) { T((T_CALLED("mvinch(%d,%d)"), a1, z)); returnChtype((wmove(stdscr,a1,z) == (-1) ? (chtype)((-1)) : winch(stdscr))); } NCURSES_EXPORT(int) (mvinchnstr) (int a1, int a2, chtype * a3, int z) { T((T_CALLED("mvinchnstr(%d,%d,%p,%d)"), a1, a2, (const void *)a3, z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : winchnstr(stdscr,a3,z))); } NCURSES_EXPORT(int) (mvinchstr) (int a1, int a2, chtype * z) { T((T_CALLED("mvinchstr(%d,%d,%p)"), a1, a2, (const void *)z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : winchnstr(stdscr, z, -1))); } NCURSES_EXPORT(int) (mvinnstr) (int a1, int a2, char * a3, int z) { return (wmove(stdscr,a1,a2) == (-1) ? (-1) : winnstr(stdscr,a3,z)) ; } NCURSES_EXPORT(int) (mvinsch) (int a1, int a2, chtype z) { T((T_CALLED("mvinsch(%d,%d,%s)"), a1, a2, _tracechtype2(2,z))); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : winsch(stdscr,z))); } NCURSES_EXPORT(int) (mvinsnstr) (int a1, int a2, const char * a3, int z) { T((T_CALLED("mvinsnstr(%d,%d,%s,%d)"), a1, a2, _nc_visbuf2(2,a3), z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : winsnstr(stdscr,a3,z))); } NCURSES_EXPORT(int) (mvinsstr) (int a1, int a2, const char * z) { T((T_CALLED("mvinsstr(%d,%d,%s)"), a1, a2, _nc_visbuf2(2,z))); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : winsnstr(stdscr, z, -1))); } NCURSES_EXPORT(int) (mvinstr) (int a1, int a2, char * z) { T((T_CALLED("mvinstr(%d,%d,%s)"), a1, a2, _nc_visbuf2(2,z))); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : winnstr(stdscr, z, -1))); } NCURSES_EXPORT(int) (mvvline) (int a1, int a2, chtype a3, int z) { T((T_CALLED("mvvline(%d,%d,%s,%d)"), a1, a2, _tracechtype2(2,a3), z)); returnCode((wmove(stdscr,a1,a2) == (-1) ? (-1) : wvline(stdscr,a3,z))); } NCURSES_EXPORT(int) (mvwaddch) (WINDOW * a1, int a2, int a3, const chtype z) { T((T_CALLED("mvwaddch(%p,%d,%d,%s)"), (const void *)a1, a2, a3, _tracechtype2(3,z))); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : waddch(a1,z))); } NCURSES_EXPORT(int) (mvwaddchnstr) (WINDOW * a1, int a2, int a3, const chtype * a4, int z) { T((T_CALLED("mvwaddchnstr(%p,%d,%d,%p,%d)"), (const void *)a1, a2, a3, (const void *)a4, z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : waddchnstr(a1,a4,z))); } NCURSES_EXPORT(int) (mvwaddchstr) (WINDOW * a1, int a2, int a3, const chtype * z) { T((T_CALLED("mvwaddchstr(%p,%d,%d,%p)"), (const void *)a1, a2, a3, (const void *)z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : waddchnstr(a1,z,-1))); } NCURSES_EXPORT(int) (mvwaddnstr) (WINDOW * a1, int a2, int a3, const char * a4, int z) { T((T_CALLED("mvwaddnstr(%p,%d,%d,%s,%d)"), (const void *)a1, a2, a3, _nc_visbuf2(3,a4), z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : waddnstr(a1,a4,z))); } NCURSES_EXPORT(int) (mvwaddstr) (WINDOW * a1, int a2, int a3, const char * z) { T((T_CALLED("mvwaddstr(%p,%d,%d,%s)"), (const void *)a1, a2, a3, _nc_visbuf2(3,z))); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : waddnstr(a1,z,-1))); } NCURSES_EXPORT(int) (mvwchgat) (WINDOW * a1, int a2, int a3, int a4, attr_t a5, short a6, const void * z) { T((T_CALLED("mvwchgat(%p,%d,%d,%d,%s,%d,%p)"), (const void *)a1, a2, a3, a4, _traceattr2(4,a5), a6, (const void *)z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : wchgat(a1,a4,a5,a6,z))); } NCURSES_EXPORT(int) (mvwdelch) (WINDOW * a1, int a2, int z) { T((T_CALLED("mvwdelch(%p,%d,%d)"), (const void *)a1, a2, z)); returnCode((wmove(a1,a2,z) == (-1) ? (-1) : wdelch(a1))); } NCURSES_EXPORT(int) (mvwgetch) (WINDOW * a1, int a2, int z) { T((T_CALLED("mvwgetch(%p,%d,%d)"), (const void *)a1, a2, z)); returnCode((wmove(a1,a2,z) == (-1) ? (-1) : wgetch(a1))); } NCURSES_EXPORT(int) (mvwgetnstr) (WINDOW * a1, int a2, int a3, char * a4, int z) { T((T_CALLED("mvwgetnstr(%p,%d,%d,%s,%d)"), (const void *)a1, a2, a3, _nc_visbuf2(3,a4), z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : wgetnstr(a1,a4,z))); } NCURSES_EXPORT(int) (mvwgetstr) (WINDOW * a1, int a2, int a3, char * z) { T((T_CALLED("mvwgetstr(%p,%d,%d,%s)"), (const void *)a1, a2, a3, _nc_visbuf2(3,z))); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : wgetnstr(a1, z, -1))); } NCURSES_EXPORT(int) (mvwhline) (WINDOW * a1, int a2, int a3, chtype a4, int z) { T((T_CALLED("mvwhline(%p,%d,%d,%s,%d)"), (const void *)a1, a2, a3, _tracechtype2(3,a4), z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : whline(a1,a4,z))); } NCURSES_EXPORT(chtype) (mvwinch) (WINDOW * a1, int a2, int z) { T((T_CALLED("mvwinch(%p,%d,%d)"), (const void *)a1, a2, z)); returnChtype((wmove(a1,a2,z) == (-1) ? (chtype)((-1)) : winch(a1))); } NCURSES_EXPORT(int) (mvwinchnstr) (WINDOW * a1, int a2, int a3, chtype * a4, int z) { T((T_CALLED("mvwinchnstr(%p,%d,%d,%p,%d)"), (const void *)a1, a2, a3, (const void *)a4, z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : winchnstr(a1,a4,z))); } NCURSES_EXPORT(int) (mvwinchstr) (WINDOW * a1, int a2, int a3, chtype * z) { T((T_CALLED("mvwinchstr(%p,%d,%d,%p)"), (const void *)a1, a2, a3, (const void *)z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : winchnstr(a1, z, -1))); } NCURSES_EXPORT(int) (mvwinnstr) (WINDOW * a1, int a2, int a3, char * a4, int z) { return (wmove(a1,a2,a3) == (-1) ? (-1) : winnstr(a1,a4,z)) ; } NCURSES_EXPORT(int) (mvwinsch) (WINDOW * a1, int a2, int a3, chtype z) { T((T_CALLED("mvwinsch(%p,%d,%d,%s)"), (const void *)a1, a2, a3, _tracechtype2(3,z))); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : winsch(a1,z))); } NCURSES_EXPORT(int) (mvwinsnstr) (WINDOW * a1, int a2, int a3, const char * a4, int z) { T((T_CALLED("mvwinsnstr(%p,%d,%d,%s,%d)"), (const void *)a1, a2, a3, _nc_visbuf2(3,a4), z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : winsnstr(a1,a4,z))); } NCURSES_EXPORT(int) (mvwinsstr) (WINDOW * a1, int a2, int a3, const char * z) { T((T_CALLED("mvwinsstr(%p,%d,%d,%s)"), (const void *)a1, a2, a3, _nc_visbuf2(3,z))); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : winsnstr(a1, z, -1))); } NCURSES_EXPORT(int) (mvwinstr) (WINDOW * a1, int a2, int a3, char * z) { T((T_CALLED("mvwinstr(%p,%d,%d,%s)"), (const void *)a1, a2, a3, _nc_visbuf2(3,z))); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : winnstr(a1, z, -1))); } NCURSES_EXPORT(int) (mvwvline) (WINDOW * a1, int a2, int a3, chtype a4, int z) { T((T_CALLED("mvwvline(%p,%d,%d,%s,%d)"), (const void *)a1, a2, a3, _tracechtype2(3,a4), z)); returnCode((wmove(a1,a2,a3) == (-1) ? (-1) : wvline(a1,a4,z))); } NCURSES_EXPORT(int) (PAIR_NUMBER) (int z) { T((T_CALLED("PAIR_NUMBER(%d)"), z)); returnCode(((int)((((unsigned long)(z) & ((((1UL) << 8) - 1UL) << ((0) + 8))) >> 8)))); } NCURSES_EXPORT(int) (redrawwin) (WINDOW * z) { T((T_CALLED("redrawwin(%p)"), (const void *)z)); returnCode(wredrawln(z, 0, (z)->_maxy+1)); } NCURSES_EXPORT(int) (refresh) (void) { T((T_CALLED("refresh()"))); returnCode(wrefresh(stdscr)); } NCURSES_EXPORT(int) (scrl) (int z) { T((T_CALLED("scrl(%d)"), z)); returnCode(wscrl(stdscr,z)); } NCURSES_EXPORT(int) (scroll) (WINDOW * z) { T((T_CALLED("scroll(%p)"), (const void *)z)); returnCode(wscrl(z,1)); } NCURSES_EXPORT(int) (setscrreg) (int a1, int z) { T((T_CALLED("setscrreg(%d,%d)"), a1, z)); returnCode(wsetscrreg(stdscr,a1,z)); } #if USE_WIDEC_SUPPORT NCURSES_EXPORT(int) (slk_attr_off) (const attr_t a1, void * z) { T((T_CALLED("slk_attr_off(%s,%p)"), _traceattr2(0,a1), (const void *)z)); returnCode(((z) ? (-1) : slk_attroff(a1))); } #endif #if USE_WIDEC_SUPPORT NCURSES_EXPORT(int) (slk_attr_on) (attr_t a1, void * z) { T((T_CALLED("slk_attr_on(%s,%p)"), _traceattr2(0,a1), (const void *)z)); returnCode(((z) ? (-1) : slk_attron(a1))); } #endif NCURSES_EXPORT(int) (standout) (void) { T((T_CALLED("standout()"))); returnIntAttr((attr_t)(((stdscr) ? ((stdscr)->_attrs = (attr_t)(((1UL) << ((8) + 8))), (0)) : (-1)))); } NCURSES_EXPORT(int) (standend) (void) { T((T_CALLED("standend()"))); returnIntAttr((attr_t)(((stdscr) ? ((stdscr)->_attrs = (attr_t)((1UL - 1UL)), (0)) : (-1)))); } NCURSES_EXPORT(void) (timeout) (int z) { T((T_CALLED("timeout(%d)"), z)); wtimeout(stdscr,z); returnVoid; } NCURSES_EXPORT(int) (touchline) (WINDOW * a1, int a2, int z) { T((T_CALLED("touchline(%p,%d,%d)"), (const void *)a1, a2, z)); returnCode(wtouchln((a1), a2, z, 1)); } NCURSES_EXPORT(int) (touchwin) (WINDOW * z) { T((T_CALLED("touchwin(%p)"), (const void *)z)); returnCode(wtouchln((z), 0, ((z) ? ((z)->_maxy + 1) : (-1)), 1)); } NCURSES_EXPORT(int) (untouchwin) (WINDOW * z) { T((T_CALLED("untouchwin(%p)"), (const void *)z)); returnCode(wtouchln((z), 0, ((z) ? ((z)->_maxy + 1) : (-1)), 0)); } NCURSES_EXPORT(int) (vline) (chtype a1, int z) { T((T_CALLED("vline(%s,%d)"), _tracechtype2(0,a1), z)); returnCode(wvline(stdscr, a1, z)); } NCURSES_EXPORT(int) (vw_printw) (WINDOW * a1, const char * a2, va_list z) { T((T_CALLED("vw_printw(%p,%s,%s)"), (const void *)a1, _nc_visbuf2(1,a2), "va_list")); returnCode(vwprintw(a1, a2, z)); } NCURSES_EXPORT(int) (vw_scanw) (WINDOW * a1, char * a2, va_list z) { T((T_CALLED("vw_scanw(%p,%s,%s)"), (const void *)a1, _nc_visbuf2(1,a2), "va_list")); returnCode(vwscanw(a1, a2, z)); } NCURSES_EXPORT(int) (waddchstr) (WINDOW * a1, const chtype * z) { T((T_CALLED("waddchstr(%p,%p)"), (const void *)a1, (const void *)z)); returnCode(waddchnstr(a1,z,-1)); } NCURSES_EXPORT(int) (waddstr) (WINDOW * a1, const char * z) { T((T_CALLED("waddstr(%p,%s)"), (const void *)a1, _nc_visbuf2(1,z))); returnCode(waddnstr(a1,z,-1)); } NCURSES_EXPORT(int) (wattron) (WINDOW * a1, int z) { T((T_CALLED("wattron(%p,%d)"), (const void *)a1, z)); returnCode(wattr_on(a1, (attr_t)(z), # 621 "_22677.c" 3 4 ((void *)0) # 621 "_22677.c" )); } NCURSES_EXPORT(int) (wattroff) (WINDOW * a1, int z) { T((T_CALLED("wattroff(%p,%d)"), (const void *)a1, z)); returnCode(wattr_off(a1, (attr_t)(z), # 627 "_22677.c" 3 4 ((void *)0) # 627 "_22677.c" )); } NCURSES_EXPORT(int) (wattrset) (WINDOW * a1, int z) { T((T_CALLED("wattrset(%p,%d)"), (const void *)a1, z)); returnIntAttr((attr_t)((a1) ? ((a1)->_attrs = (attr_t)(z), (0)) : (-1))); } NCURSES_EXPORT(int) (wattr_get) (WINDOW * a1, attr_t * a2, short * a3, void * z) { T((T_CALLED("wattr_get(%p,%p,%p,%p)"), (const void *)a1, (const void *)a2, (const void *)a3, (const void *)z)); returnCode(((void)((a2) != (void *)0 && (*(a2) = (a1)->_attrs)), (void)((a3) != (void *)0 && (*(a3) = (short)((int)((((unsigned long)((a1)->_attrs) & ((((1UL) << 8) - 1UL) << ((0) + 8))) >> 8))))), (0))); } NCURSES_EXPORT(int) (wattr_set) (WINDOW * a1, attr_t a2, short a3, void * z) { T((T_CALLED("wattr_set(%p,%s,%d,%p)"), (const void *)a1, _traceattr2(1,a2), a3, (const void *)z)); returnCode(((a1)->_attrs = (((a2) & ~((((1UL) << 8) - 1UL) << ((0) + 8))) | (attr_t)((a3) << ((0) + 8))), (0))); } NCURSES_EXPORT(int) (wdeleteln) (WINDOW * z) { T((T_CALLED("wdeleteln(%p)"), (const void *)z)); returnCode(winsdelln(z,-1)); } NCURSES_EXPORT(int) (wgetstr) (WINDOW * a1, char * z) { T((T_CALLED("wgetstr(%p,%s)"), (const void *)a1, _nc_visbuf2(1,z))); returnCode(wgetnstr(a1, z, -1)); } NCURSES_EXPORT(int) (winchstr) (WINDOW * a1, chtype * z) { T((T_CALLED("winchstr(%p,%p)"), (const void *)a1, (const void *)z)); returnCode(winchnstr(a1, z, -1)); } NCURSES_EXPORT(int) (winsertln) (WINDOW * z) { T((T_CALLED("winsertln(%p)"), (const void *)z)); returnCode(winsdelln(z,1)); } NCURSES_EXPORT(int) (winsstr) (WINDOW * a1, const char * z) { T((T_CALLED("winsstr(%p,%s)"), (const void *)a1, _nc_visbuf2(1,z))); returnCode(winsnstr(a1, z, -1)); } NCURSES_EXPORT(int) (winstr) (WINDOW * a1, char * z) { T((T_CALLED("winstr(%p,%s)"), (const void *)a1, _nc_visbuf2(1,z))); returnCode(winnstr(a1, z, -1)); } NCURSES_EXPORT(int) (wstandout) (WINDOW * z) { T((T_CALLED("wstandout(%p)"), (const void *)z)); returnIntAttr((attr_t)(((z) ? ((z)->_attrs = (attr_t)(((1UL) << ((8) + 8))), (0)) : (-1)))); } NCURSES_EXPORT(int) (wstandend) (WINDOW * z) { T((T_CALLED("wstandend(%p)"), (const void *)z)); returnIntAttr((attr_t)(((z) ? ((z)->_attrs = (attr_t)((1UL - 1UL)), (0)) : (-1)))); } NCURSES_EXPORT(int) (getattrs) (const WINDOW * z) { T((T_CALLED("getattrs(%p)"), (const void *)z)); returnCode((int)((z) ? (z)->_attrs : (1UL - 1UL))); } NCURSES_EXPORT(int) (getcurx) (const WINDOW * z) { T((T_CALLED("getcurx(%p)"), (const void *)z)); returnCode(((z) ? (z)->_curx : (-1))); } NCURSES_EXPORT(int) (getcury) (const WINDOW * z) { T((T_CALLED("getcury(%p)"), (const void *)z)); returnCode(((z) ? (z)->_cury : (-1))); } NCURSES_EXPORT(int) (getbegx) (const WINDOW * z) { T((T_CALLED("getbegx(%p)"), (const void *)z)); returnCode(((z) ? (z)->_begx : (-1))); } NCURSES_EXPORT(int) (getbegy) (const WINDOW * z) { T((T_CALLED("getbegy(%p)"), (const void *)z)); returnCode(((z) ? (z)->_begy : (-1))); } NCURSES_EXPORT(int) (getmaxx) (const WINDOW * z) { T((T_CALLED("getmaxx(%p)"), (const void *)z)); returnCode(((z) ? ((z)->_maxx + 1) : (-1))); } NCURSES_EXPORT(int) (getmaxy) (const WINDOW * z) { T((T_CALLED("getmaxy(%p)"), (const void *)z)); returnCode(((z) ? ((z)->_maxy + 1) : (-1))); } NCURSES_EXPORT(int) (getparx) (const WINDOW * z) { T((T_CALLED("getparx(%p)"), (const void *)z)); returnCode(((z) ? (z)->_parx : (-1))); } NCURSES_EXPORT(int) (getpary) (const WINDOW * z) { T((T_CALLED("getpary(%p)"), (const void *)z)); returnCode(((z) ? (z)->_pary : (-1))); } NCURSES_EXPORT(WINDOW *) (wgetparent) (const WINDOW * z) { T((T_CALLED("wgetparent(%p)"), (const void *)z)); returnWin(((z) ? (z)->_parent : 0)); } # 757 "_22677.c" 3 4 NCURSES_BOOL # 757 "_22677.c" NCURSES_EXPORT() (is_cleared) (const WINDOW * z) { T((T_CALLED("is_cleared(%p)"), (const void *)z)); returnBool(((z) ? (z)->_clear : 0)); } # 763 "_22677.c" 3 4 NCURSES_BOOL # 763 "_22677.c" NCURSES_EXPORT() (is_idcok) (const WINDOW * z) { T((T_CALLED("is_idcok(%p)"), (const void *)z)); returnBool(((z) ? (z)->_idcok : 0)); } # 769 "_22677.c" 3 4 NCURSES_BOOL # 769 "_22677.c" NCURSES_EXPORT() (is_idlok) (const WINDOW * z) { T((T_CALLED("is_idlok(%p)"), (const void *)z)); returnBool(((z) ? (z)->_idlok : 0)); } # 775 "_22677.c" 3 4 NCURSES_BOOL # 775 "_22677.c" NCURSES_EXPORT() (is_immedok) (const WINDOW * z) { T((T_CALLED("is_immedok(%p)"), (const void *)z)); returnBool(((z) ? (z)->_immed : 0)); } # 781 "_22677.c" 3 4 NCURSES_BOOL # 781 "_22677.c" NCURSES_EXPORT() (is_keypad) (const WINDOW * z) { T((T_CALLED("is_keypad(%p)"), (const void *)z)); returnBool(((z) ? (z)->_use_keypad : 0)); } # 787 "_22677.c" 3 4 NCURSES_BOOL # 787 "_22677.c" NCURSES_EXPORT() (is_leaveok) (const WINDOW * z) { T((T_CALLED("is_leaveok(%p)"), (const void *)z)); returnBool(((z) ? (z)->_leaveok : 0)); } # 793 "_22677.c" 3 4 NCURSES_BOOL # 793 "_22677.c" NCURSES_EXPORT() (is_nodelay) (const WINDOW * z) { T((T_CALLED("is_nodelay(%p)"), (const void *)z)); returnBool(((z) ? ((z)->_delay == 0) : 0)); } # 799 "_22677.c" 3 4 NCURSES_BOOL # 799 "_22677.c" NCURSES_EXPORT() (is_notimeout) (const WINDOW * z) { T((T_CALLED("is_notimeout(%p)"), (const void *)z)); returnBool(((z) ? (z)->_notimeout : 0)); } # 805 "_22677.c" 3 4 NCURSES_BOOL # 805 "_22677.c" NCURSES_EXPORT() (is_pad) (const WINDOW * z) { T((T_CALLED("is_pad(%p)"), (const void *)z)); returnBool(((z) ? ((z)->_flags & 0x10) != 0 : 0)); } # 811 "_22677.c" 3 4 NCURSES_BOOL # 811 "_22677.c" NCURSES_EXPORT() (is_scrollok) (const WINDOW * z) { T((T_CALLED("is_scrollok(%p)"), (const void *)z)); returnBool(((z) ? (z)->_scroll : 0)); } # 817 "_22677.c" 3 4 NCURSES_BOOL # 817 "_22677.c" NCURSES_EXPORT() (is_subwin) (const WINDOW * z) { T((T_CALLED("is_subwin(%p)"), (const void *)z)); returnBool(((z) ? ((z)->_flags & 0x01) != 0 : 0)); } # 823 "_22677.c" 3 4 NCURSES_BOOL # 823 "_22677.c" NCURSES_EXPORT() (is_syncok) (const WINDOW * z) { T((T_CALLED("is_syncok(%p)"), (const void *)z)); returnBool(((z) ? (z)->_sync : 0)); } NCURSES_EXPORT(int) (wgetscrreg) (const WINDOW * a1, int * a2, int * z) { T((T_CALLED("wgetscrreg(%p,%p,%p)"), (const void *)a1, (const void *)a2, (const void *)z)); returnCode(((a1) ? (*(a2) = (a1)->_regtop, *(z) = (a1)->_regbottom, (0)) : (-1))); } # 835 "_22677.c" 3 4 NCURSES_BOOL # 835 "_22677.c" mouse_trafo (int * a1, int * a2, # 835 "_22677.c" 3 4 NCURSES_BOOL # 835 "_22677.c" z) { T((T_CALLED("mouse_trafo(%p,%p,%#lx)"), (const void *)a1, (const void *)a2, (long)z)); returnBool(wmouse_trafo(stdscr,a1,a2,z)); }
Hi gangyu li,
Since the original issue is on H264 decoding and now you have issue with yocto building, can you please raise a new e2e thread ?
It will be notified to correct person to address the issue.
Thanks
Ramprasad
Hi Ramprasad
Building Yocto Filesystem Error Please Help Solve。
log:
yj@localhost:~/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers$ ./build-core-sdk.sh dra7xx-evm
In which directory do you want to place the downloads for the Yocto build ?(if this directory does not exist it will be created)
Ensure that complete path is provided.
[ /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/downloads ]
[GLSDK]>
[GLSDK]> Current Directory is /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers
[GLSDK]> PATH is /home/yj/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux/bin:/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/bin:/home/yj/bin:/home/yj/.local/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin
[GLSDK]> Building on localhost.localdomain running Linux localhost.localdomain 4.15.0-54-generic #58~16.04.1-Ubuntu SMP Mon Jun 24 13:21:41 UTC 2019 x86_64 x86_64 x86_64 GNU/Linux
[GLSDK]> Starting Yocto build at 2019年 07月 11日 星期四 18:29:57 CST
[GLSDK]>
[GLSDK]> ./oe-layertool-setup.sh -f configs/glsdk/glsdk-7.02.00.02-config.txt
/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers
cloning repo bitbake
正在获取 origin
之前的 HEAD 位置是 fbf1c39... lib/bb/utils: add safeguard against recursively deleting things we shouldn't
切换到分支 '1.24'
您的分支与上游分支 'origin/1.24' 一致。
Already up-to-date.
Note: checking out 'fbf1c39641f78d553961974a2bb96256eb9496e7'.
You are in 'detached HEAD' state. You can look around, make experimental
changes and commit them, and you can discard any commits you make in this
state without impacting any branches by performing another checkout.
If you want to create a new branch to retain commits you create, you may
do so (now or later) by using -b with the checkout command again. Example:
git checkout -b <new-branch-name>
HEAD 目前位于 fbf1c39... lib/bb/utils: add safeguard against recursively deleting things we shouldn't
cloning repo meta-glsdk
正在获取 origin
之前的 HEAD 位置是 5ed9ab7... glsdk-example-apps: Update to include bandwidth-tool
切换到分支 'master'
您的分支与上游分支 'origin/master' 一致。
Already up-to-date.
Note: checking out '5ed9ab72fb1c0e2bc3b1bd4d508c972bf2b21b0e'.
You are in 'detached HEAD' state. You can look around, make experimental
changes and commit them, and you can discard any commits you make in this
state without impacting any branches by performing another checkout.
If you want to create a new branch to retain commits you create, you may
do so (now or later) by using -b with the checkout command again. Example:
git checkout -b <new-branch-name>
HEAD 目前位于 5ed9ab7... glsdk-example-apps: Update to include bandwidth-tool
cloning repo meta-arago
正在获取 origin
之前的 HEAD 位置是 dc89e06... libdce: update to 3.00.08.02
切换到分支 'master'
您的分支与上游分支 'origin/master' 一致。
Already up-to-date.
Note: checking out 'dc89e06d2a64f33d9e9662e6f7fe1f8466ff167c'.
You are in 'detached HEAD' state. You can look around, make experimental
changes and commit them, and you can discard any commits you make in this
state without impacting any branches by performing another checkout.
If you want to create a new branch to retain commits you create, you may
do so (now or later) by using -b with the checkout command again. Example:
git checkout -b <new-branch-name>
HEAD 目前位于 dc89e06... libdce: update to 3.00.08.02
cloning repo meta-qt5
正在获取 origin
切换到分支 'daisy'
您的分支与上游分支 'origin/daisy' 一致。
Already up-to-date.
Note: checking out '23405d3a66c308e0b2ea64308b834285850c5c9f'.
You are in 'detached HEAD' state. You can look around, make experimental
changes and commit them, and you can discard any commits you make in this
state without impacting any branches by performing another checkout.
If you want to create a new branch to retain commits you create, you may
do so (now or later) by using -b with the checkout command again. Example:
git checkout -b <new-branch-name>
HEAD 目前位于 23405d3... qt5-git: Fetch from code.qt.io
cloning repo meta-openembedded
正在获取 origin
切换到分支 'daisy'
您的分支与上游分支 'origin/daisy' 一致。
Already up-to-date.
Note: checking out 'd3d14d3fcca7fcde362cf0b31411dc4eea6d20aa'.
You are in 'detached HEAD' state. You can look around, make experimental
changes and commit them, and you can discard any commits you make in this
state without impacting any branches by performing another checkout.
If you want to create a new branch to retain commits you create, you may
do so (now or later) by using -b with the checkout command again. Example:
git checkout -b <new-branch-name>
HEAD 目前位于 d3d14d3... gdal: fix sqlite, expat and libtiff detection
cloning repo meta-ti
正在获取 origin
切换到分支 'daisy'
您的分支与上游分支 'origin/daisy' 一致。
Already up-to-date.
Note: checking out '090b02a104924886afd0fa79be7b5d08eebf071f'.
You are in 'detached HEAD' state. You can look around, make experimental
changes and commit them, and you can discard any commits you make in this
state without impacting any branches by performing another checkout.
If you want to create a new branch to retain commits you create, you may
do so (now or later) by using -b with the checkout command again. Example:
git checkout -b <new-branch-name>
HEAD 目前位于 090b02a... uio-module-drv: Update to new version 1.0.2.3
cloning repo meta-linaro
正在获取 origin
之前的 HEAD 位置是 0600823... eglibc-linaro: Sync patches from OE-Core
切换到分支 'daisy'
您的分支与上游分支 'origin/daisy' 一致。
Already up-to-date.
Note: checking out '06008235ca752fea678953e85adaa29a491d246b'.
You are in 'detached HEAD' state. You can look around, make experimental
changes and commit them, and you can discard any commits you make in this
state without impacting any branches by performing another checkout.
If you want to create a new branch to retain commits you create, you may
do so (now or later) by using -b with the checkout command again. Example:
git checkout -b <new-branch-name>
HEAD 目前位于 0600823... eglibc-linaro: Sync patches from OE-Core
cloning repo oe-core
正在获取 origin
之前的 HEAD 位置是 e1a2540... squashfs-tools: enable building unsquashfs and fix squashfs-4.2-fix-CVE-2012-4025.patch
切换到分支 'daisy'
您的分支与上游分支 'origin/daisy' 一致。
Already up-to-date.
Note: checking out 'e1a2540227250d854d5bba278634bcc9e7572cda'.
You are in 'detached HEAD' state. You can look around, make experimental
changes and commit them, and you can discard any commits you make in this
state without impacting any branches by performing another checkout.
If you want to create a new branch to retain commits you create, you may
do so (now or later) by using -b with the checkout command again. Example:
git checkout -b <new-branch-name>
HEAD 目前位于 e1a2540... squashfs-tools: enable building unsquashfs and fix squashfs-4.2-fix-CVE-2012-4025.patch
################################################################################
The bblayers.conf configuration file has been created for you with some
default values. Please verify the contents of your conf/bblayers.conf
file for correctness.
NOTE: Any additional entries to this file will be lost if the ./oe-layertool-setup.sh
script is run again. To add entries permanently to this file
please add them to the config file used and rerun the
./oe-layertool-setup.sh script.
################################################################################
The local.conf configuration file has been created for you with some
default values. Please verify the contents of your conf/local.conf
file for correctness.
By default the number of threads used by the build is set to the number
of CPUs found on your system.
NOTE: You will probably want to change the default MACHINE setting in the
local.conf file to the machine you are trying to build.
WARNING: Found existing /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/conf/local.conf
Saving a backup to /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/conf/local.conf.bak
################################################################################
A setenv file has been created for you in the conf directory. Please verify
The contents of this file. Once you have verified the contents please source
this file to configure your environment for building:
. conf/setenv
You can then start building using the bitbake command. You will likely want
to set the MACHINE option if you have not done so in your local.conf file.
For example:
MACHINE=xxxxx bitbake <target>
Common targets are:
core-image-minimal
core-image-sato
meta-toolchain
meta-toolchain-sdk
adt-installer
meta-ide-support
/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02 ====== cyj
[GLSDK]> cd build
[GLSDK]> . conf/setenv
[GLSDK]> cp conf/local.conf conf/local.conf.pristine
[GLSDK]> echo ARAGO_BRAND = "glsdk" >> conf/local.conf
[GLSDK]> MACHINE=dra7xx-evm bitbake arago-glsdk-multimedia-image
NOTE: Started PRServer with DBfile: /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 38859, PID: 19066
Loading cache: 100% |#################################################################################################################################| ETA: 00:00:00
Loaded 2251 entries from dependency cache.
Parsing recipes: 100% |###############################################################################################################################| Time: 00:00:04
Parsing of 1807 .bb files complete (1518 cached, 289 parsed). 2250 targets, 210 skipped, 0 masked, 0 errors.
WARNING: No recipes available for:
/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/sources/meta-arago/meta-arago-distro/recipes-qt/qt5/qtbase_5.4.1.bbappend
/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/sources/meta-arago/meta-arago-distro/recipes-connectivity/openssl/openssl_1.0.1m.bbappend
/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/sources/meta-arago/meta-arago-distro/recipes-qt/qt5/qtwebkit_5.4.1.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.24.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "dra7xx-evm"
DISTRO = "arago"
DISTRO_VERSION = "2013.10"
TUNE_FEATURES = "armv7a vfp thumb neon callconvention-hard cortexa15"
TARGET_FPU = "vfp-neon"
meta-glsdk = "(HEADdetachedat5ed9ab7):5ed9ab72fb1c0e2bc3b1bd4d508c972bf2b21b0e"
meta-arago-distro
meta-arago-extras = "(HEADdetachedatdc89e06):dc89e06d2a64f33d9e9662e6f7fe1f8466ff167c"
meta-qt5 = "(HEADdetachedat23405d3):23405d3a66c308e0b2ea64308b834285850c5c9f"
toolchain-layer
meta-networking
meta-ruby
meta-oe = "(HEADdetachedatd3d14d3):d3d14d3fcca7fcde362cf0b31411dc4eea6d20aa"
meta-ti = "(HEADdetachedat090b02a):090b02a104924886afd0fa79be7b5d08eebf071f"
meta-linaro-toolchain = "(HEADdetachedat0600823):06008235ca752fea678953e85adaa29a491d246b"
meta = "(HEADdetachedate1a2540):e1a2540227250d854d5bba278634bcc9e7572cda"
NOTE: Preparing runqueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Function failed: do_compile (log file is located at /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/temp/log.do_compile.19201)
ERROR: Logfile of failure stored in: /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/temp/log.do_compile.19201
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 8 -C narrowc libs
| make: Entering directory '/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/build/narrowc'
| cd include && make DESTDIR="" libs
| make[1]: Entering directory '/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/build/narrowc/include'
| make[1]: Nothing to be done for 'libs'.
| make[1]: Leaving directory '/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/build/narrowc/include'
| cd ncurses && make DESTDIR="" libs
| make[1]: Entering directory '/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/build/narrowc/ncurses'
| linking ../lib/libtinfo.so.5.9
| gcc -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -O2 -pipe --param max-inline-insns-single=1200 -shared -Wl,-soname,`basename ../lib/libtinfo.so.5.9 .5.9`.5,-stats,-lc -o ../lib/libtinfo.so.5.9 ../obj_s/access.o ../obj_s/add_tries.o ../obj_s/alloc_ttype.o ../obj_s/codes.o ../obj_s/comp_captab.o ../obj_s/comp_error.o ../obj_s/comp_hash.o ../obj_s/db_iterator.o ../obj_s/doalloc.o ../obj_s/entries.o ../obj_s/fallback.o ../obj_s/free_ttype.o ../obj_s/getenv_num.o ../obj_s/home_terminfo.o ../obj_s/init_keytry.o ../obj_s/lib_acs.o ../obj_s/lib_baudrate.o ../obj_s/lib_cur_term.o ../obj_s/lib_data.o ../obj_s/lib_has_cap.o ../obj_s/lib_kernel.o ../obj_s/lib_keyname.o ../obj_s/lib_longname.o ../obj_s/lib_napms.o ../obj_s/lib_options.o ../obj_s/lib_raw.o ../obj_s/lib_setup.o ../obj_s/lib_termcap.o ../obj_s/lib_termname.o ../obj_s/lib_tgoto.o ../obj_s/lib_ti.o ../obj_s/lib_tparm.o ../obj_s/lib_tputs.o ../obj_s/lib_trace.o ../obj_s/lib_ttyflags.o ../obj_s/lib_twait.o ../obj_s/name_match.o ../obj_s/names.o ../obj_s/read_entry.o ../obj_s/read_termcap.o ../obj_s/setbuf.o ../obj_s/strings.o ../obj_s/tries.o ../obj_s/trim_sgr0.o ../obj_s/unctrl.o ../obj_s/visbuf.o ../obj_s/define_key.o ../obj_s/hashed_db.o ../obj_s/key_defined.o ../obj_s/keybound.o ../obj_s/keyok.o ../obj_s/version.o -L../lib -L/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/lib -L/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/lib -Wl,-rpath-link,/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/lib -Wl,-rpath-link,/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/lib -Wl,-rpath,/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/lib -Wl,-rpath,/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/lib -Wl,-O1
| gcc -DHAVE_CONFIG_H -I../ncurses -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -DNDEBUG -I. -I../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -O2 -pipe --param max-inline-insns-single=1200 -fPIC -c ../ncurses/lib_gen.c -o ../obj_s/lib_gen.o
| gcc -DHAVE_CONFIG_H -I../ncurses -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -DNDEBUG -I. -I../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -O2 -pipe --param max-inline-insns-single=1200 -c ../ncurses/lib_gen.c -o ../objects/lib_gen.o
| gcc -DHAVE_CONFIG_H -I../ncurses -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -DNDEBUG -I. -I../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -O2 -pipe --param max-inline-insns-single=1200 -c /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/base/lib_isendwin.c -o ../objects/lib_isendwin.o
| gcc -DHAVE_CONFIG_H -I../ncurses -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -DNDEBUG -I. -I../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -O2 -pipe --param max-inline-insns-single=1200 -c /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/base/lib_leaveok.c -o ../objects/lib_leaveok.o
| gcc -DHAVE_CONFIG_H -I../ncurses -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -DNDEBUG -I. -I../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -O2 -pipe --param max-inline-insns-single=1200 -c /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/base/lib_mouse.c -o ../objects/lib_mouse.o
| gcc -DHAVE_CONFIG_H -I../ncurses -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -DNDEBUG -I. -I../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -O2 -pipe --param max-inline-insns-single=1200 -c /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/base/lib_move.c -o ../objects/lib_move.o
| gcc -DHAVE_CONFIG_H -I../ncurses -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -DNDEBUG -I. -I../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -O2 -pipe --param max-inline-insns-single=1200 -c /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/tty/lib_mvcur.c -o ../objects/lib_mvcur.o
| /usr/bin/ld: total time in link: 0.026598
| /usr/bin/ld: data size 5160960
| cd ../lib && (ln -s -f libtinfo.so.5.9 libtinfo.so.5; ln -s -f libtinfo.so.5 libtinfo.so; )
| In file included from /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/curses.priv.h:283:0,
| from ../ncurses/lib_gen.c:19:
| _30006.c:835:15: error: expected ')' before 'int'
| ../include/curses.h:1594:56: note: in definition of macro 'mouse_trafo'
| #define mouse_trafo(y,x,to_screen) wmouse_trafo(stdscr,y,x,to_screen)
| ^
| gcc -DHAVE_CONFIG_H -I../ncurses -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -DNDEBUG -I. -I../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/../include -I/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -isystem/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include -D_GNU_SOURCE -O2 -pipe --param max-inline-insns-single=1200 -c /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/base/lib_mvwin.c -o ../objects/lib_mvwin.o
| In file included from /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/ncurses-5.9/ncurses/curses.priv.h:283:0,
| from ../ncurses/lib_gen.c:19:
| _30006.c:835:15: error: expected ')' before 'int'
| ../include/curses.h:1594:56: note: in definition of macro 'mouse_trafo'
| #define mouse_trafo(y,x,to_screen) wmouse_trafo(stdscr,y,x,to_screen)
| ^
| Makefile:1682: recipe for target '../obj_s/lib_gen.o' failed
| make[1]: *** [../obj_s/lib_gen.o] Error 1
| make[1]: *** Waiting for unfinished jobs....
| Makefile:2202: recipe for target '../objects/lib_gen.o' failed
| make[1]: *** [../objects/lib_gen.o] Error 1
| make[1]: Leaving directory '/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/build/narrowc/ncurses'
| Makefile:134: recipe for target 'libs' failed
| make: *** [libs] Error 2
| make: Leaving directory '/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/build/narrowc'
| ERROR: oe_runmake failed
| WARNING: /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/temp/run.do_compile.19201:1 exit 1 from
| exit 1
| ERROR: Function failed: do_compile (log file is located at /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ncurses-native/5.9-r15.1/temp/log.do_compile.19201)
ERROR: Task 500 (virtual:native:/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/sources/oe-core/meta/recipes-core/ncurses/ncurses_5.9.bb, do_compile) failed with exit code '1'
WARNING: Failed to fetch URL releases.linaro.org/.../binutils-linaro-2.24-2014.03.tar.xz, attempting MIRRORS if available
ERROR: Fetcher failure: Fetch command failed with exit code 8, output:
releases.linaro.org/.../binutils-linaro-2.24-2014.03.tar.xz:
2019-07-11 18:30:27 ERROR 404: Not Found.
ERROR: Function failed: Fetcher failure for URL: 'releases.linaro.org/.../binutils-linaro-2.24-2014.03.tar.xz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/linaro-2.24-r2014.03/temp/log.do_fetch.19203
ERROR: Task 600 (virtual:native:/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/binutils/binutils_linaro-2.24.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 218 tasks of which 207 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
Waiting for 0 running tasks to finish:
Summary: 2 tasks failed:
virtual:native:/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/sources/oe-core/meta/recipes-core/ncurses/ncurses_5.9.bb, do_compile
virtual:native:/home/yj/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/binutils/binutils_linaro-2.24.bb, do_fetch
Summary: There were 2 WARNING messages shown.
Summary: There were 3 ERROR messages shown, returning a non-zero exit code.
[GLSDK]>
[GLSDK]> Completed Yocto build at 2019年 07月 11日 星期四 18:30:38 CST
[GLSDK]>
yj@localhost:~/ti-glsdk_dra7xx-evm_7_02_00_02/yocto-layers$
I have read your excellent post. This is a great job. I have enjoyed reading your post first time.