I am using an AM4379 on an AM437x-IDK-EVM to boot over the network interface, ETH0. The configuration pins on the AM4379 have been modified (using the 0ohm resisters on the board.) for the following configuration.
The AM437x-IDK-EVM board is connected to a network interface with bootp server (Ubuntu host) that has dhcpd and tftp sever started. The dhcp conf file is shown below:
When the AM327X-IDK-EVM is powered on it makes a bootp request and the bootp server responds but the AM437x-IDK-EVM does request the u-boot-spl.bin file from the tftp server?
I have the WireShark capture of the two packets highlighted above, but I do not seem be able to attach it to this message?
I have used this Ubuntu server to boot another AM437x-IDK-EVM and it worked as expected, this EVM however appears to be interfacing/booting from the server differently?
Is there a field in the Boot Reply that I may be missing that is not allowing this device to boot? (for example another Next Server type field or a Tftp server field?)
Thanks in advance,
Rob