Hi,
In TIDL_OD demo, the target recognition is classified as follows:
typedef enum
{
TI_OD_PEDESTRIAN = 0,
TI_OD_TRAFFIC_SIGN,
TI_OD_VEHICLE,
TI_OD_MAX_OBJECTS
} TI_OD_ObjectType;
I am now have a car and traffic sign(only speed limit sign 30,40,50,60,80,100) recognition task, and My classification is as follows:
But there are objSubType in the property list as follows:
How do I attribute my speed limit sign classification to TSR?
{
uint32_t objTag;
uint32_t objType;
uint32_t objSubType;
uint32_t xPos;
uint32_t yPos;
uint32_t objWidth;
uint32_t objHeight;
float objScore;
float objScale;
float reserved0;
float reserved1;
float reserved2;
} TI_OD_objectDescriptor;