Tool/software: Linux
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi
Linux version:linux 4.4.117
software and hardware environment:
OS Kernel: | Linux® 4.4.117 |
---|---|
Android: | Android™ Oreo™ MR1 8.1 (OPM1.171019.021) |
Toolchain: | Android linux-x86 toolchain android-eabi-4.9 |
Supported J6 Platforms: | J6 EVM (REV H), J6 Eco EVM (Rev C), J6 Entry EVM, and J6 Plus EVM |
IPC Version: | 3.47.01.00 |
Build Host OS: | Ubuntu 64 bit with Java8 |
Daily Build Version: | JACINTO6_O_DB build 185 |
Hi
can you clarify the usage
Is UART1 configured and enabled as part of the device tree definition
Are you trying to enable UART1 as console and use that for logging low-level message for your custom board implementation
Lastly, is your work based on TI android SDK release, if so can clarify on the SDK version
Hi @xiao wen ,
did you had any progress on this issue?
Can you give the details asked by Sriram, so we can help you?
Regards,
Yordan
Hi
Can you confirm if you need any further help with this - will close the thread otherwise