We have a C5505 running a Mass Storage Application derived from the CSL 3.03 example. The device mounts to windows as a 512KB Mass Storage Device. Connecting the device to windows 7 everything works fine. Mounts like a flash drive and a file can be copied to it. Connecting the device to Windows 10, the device connects, allows a user to write a file to the Mass Storage Device (copy and paste a *.bin file is how it is usually performed). Windows reports everything is fine, the file says it copies 100% on the progress bar, but the application does not receive the data. Any thoughts as to what might cause this? This happens on every Windows 10 PC we have tried it on.