Hi,
this is Michael Lawnick from Nokia.
My colleague opened a question in <https://e2e.ti.com/support/processors/f/791/t/804481>
The answer by TI seemed not to be related to the problem:
We search for a method to reset CNTPCT without the need to do a power cycle. Is there a method to achieve this by software?
The underlying story: we need to monitor boot time. Our system is already delivered to customer and primary bootloader in a write protected flash device. So monitoring must base on an by-default enabled counter which either starts a zero after reset or can be set to zero before reset.
The only K2-SoC timer which is enabled by default seems to be CNTPCT.