Hi
I am trying to modify the MMCSD_FatfsConsole_lcdkOMAPL138_DMA_c674xExampleProject
to a MMCSD_BUS_WIDTH_1BIT;
I have modified the pinmux code and rebuilt the libraries
I have also added
hwAttrsConfig.supportedBusWidth=MMCSD_BUS_WIDTH_1BIT;
hwAttrsConfig.inputClk=25000000;
my serial output was:
Card inserted.
All tests have PASSED
0:>ls
I also tried MMCSD_lcdkOMAPL138_DMA_c674xTestProject
And this was my output
Test Details for test ID = 13
Test Profile[13]: Description = Default Unit Test (Max speed)
Test Profile[13]: PowerCyle = Required
Test Profile[13] Device Config : Mode = SOC Default
Test Profile[13] Device Config : BusVoltage = SOC Default
Test Profile[13] Device Config : BusWidth = SOC Default
Test Profile[13] Device Config : Interrupt = SOC Default
------------------------------------------------------------
DMA is enabled
Interrupts are disabled
Performing RAW mode read/write tests ..
SD Card: BlockSize = 512, BlockCount = 0x01ce0000, CardSize = 0x39c000000 bytes
RAW READ/WRITE: Reading test pattern (256 KB) from the SD card starting at sector 0x300000 in 1 block(s) 256 KB each
RAW READ/WRITE: PASS: Read/Write Success for this size (256 KB)
RAW READ/WRITE: Reading test pattern (512 KB) from the SD card starting at sector 0x300000 in 1 block(s) 512 KB each
RAW READ/WRITE: PASS: Read/Write Success for this size (512 KB)
RAW READ/WRITE: Reading test pattern (1024 KB) from the SD card starting at sector 0x300000 in 1 blo