This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

RTOS/PROCESSOR-SDK-OMAPL138: FTP - problems with transfer when change size of SO_RCVBUF and SO_SNDBUF

Intellectual 770 points

Replies: 11

Views: 431

Part Number: PROCESSOR-SDK-OMAPL138

Tool/software: TI-RTOS

Hello,

I'm using the latest SDK and I have a problem with FTP data transfer.

I changed the size of the send/receive buffer by using:

setsockopt(ioh->data_socket, SOL_SOCKET, SO_SNDBUF, &valSnd, sizeof(valSnd));

setsockopt(ioh->data_socket, SOL_SOCKET, SO_RCVBUF, &val, sizeof(val));

When I used default size of the the send/receiver buffer my data transfer suspended!

When I changed the size to 2048, transfer of ONE file is fine, but when I am trying send/receive more then one file my transfer suspended.

The next observation: when I changed buffer size to 1kB data transfer is OK (also for parallel transfer of more than one file), but speed transfer is very very slow!

I noticed that when my program doesn't receive the ACK form the PC it sends the frame again and in CCS CONSOLE I see (00691.900 TcpTimeoutRexmt: Retransmit Timeout), when I have a small buffer, I see the frames being sent again in Wireshark, but when I have a larger buffer I see only a retransmission frames in the CCS Console (I don't see it in Wireshark) and the transfer suspend here.

What can I do to improve my transfer?

I attach an attachment *.cfg2437.app.cfg

  • Guru 69970 points

    Hi,

    Are you able to provide the Processor SDK RTOS release version and NDK version info? Is your code based on the NIMU_FtpExample_<board>_<cpu>ExampleProject and ported to L138?

    Is this the befault setting (from .cfg):

    Tcp.transmitBufSize = 16384;
    Tcp.receiveBufSize = 65536;
    Tcp.receiveBufLimit = 65536;

    Regards, Eric

  • In reply to lding:

    Hi Eric,

    Thank you for your answer.

    I am using ti-processor-sdk-rtos-omapl138-lcdk-06.00.00.07-Windows-x86-Install.exe and this product includes ndk_3_60_00_13.

    Yes, my code is based on the NIMU_FtpExample ExampleProject and ported to OMAPL138.

    I didn't create Example Project I used files from ti\pdk_omapl138_1_0_9\packages\ti\transport\ndk\nimu\example\ftpApp\ftpserver

    Is this the befault setting (from .cfg):
    Tcp.transmitBufSize = 16384;
    Tcp.receiveBufSize = 65536;
    Tcp.receiveBufLimit = 65536;

    What is wrong with the above values?

    When I use new values in my code the values set in *.cfg are overwritten, that's right?

    Additionally, when I pull out eth plug, I noticed also retransmit but when I pull the eth plug back in, transmission continues.

    The photo shows behavior when the transmission is suspended.

    Additionally, when I disable cache all works fine also after increasing the size of the buffer but transfer speed is very low...

    Regards, Patryk

  • In reply to Patryk_93:

    Any suggestions?

  • Guru 69970 points

    In reply to Patryk_93:

    Hi,

    In general, you want to make the TCP transmitBufSize and receiveBufSize as large as the app will allow, as the size of these buffers will affect the throughput performance of a TCP connection. TCP buffer sizes (window) is capped at 64K (see TCP_MAXWIN in NDK).

    The settings in *.cfg file are configuring the default values for when any TCP socket is created. Note that the receiveBufLimit size only affects no-copy sockets (that are used with the no-copy APIs, such as recvnc() )

    • Tcp.transmitBufSize = 65536;
    • Tcp.receiveBufSize = 65536;
    • Tcp.receiveBufLimit = 65536;

    This can be overridden after the socket has been created by using the setsockopt() API, as you show in the “C code” section.

    • setsockopt(ioh->data_socket, SOL_SOCKET, SO_SNDBUF, &valSnd, sizeof(valSnd));
    • setsockopt(ioh->data_socket, SOL_SOCKET, SO_RCVBUF, &val, sizeof(val));

    I would like to suggest you keeping the cache enabled, and setting TCP TX/RX buffer with 64K and changing the buffer size using C code to get the optimized values.

    Regards, Eric 

  • In reply to lding:

    Hi Eric,

    I add to this thread new observations:

    My program works fine but see my settings:

    int val = 32768;
    int valSnd = 1500; //DON'T CHANGE!!!
    
    setsockopt(ioh->data_socket, SOL_SOCKET, SO_SNDBUF, &valSnd, sizeof(valSnd));
    setsockopt(ioh->data_socket, SOL_SOCKET, SO_RCVBUF, &val, sizeof(val));
    
    //...
    //My function to send data:
    numSent = send(connection, ioh->DataBuf, numRead, 0); //ioh->DataBuf has 32kB size

    When I increased SO_SNDBUF my send function return -1 and all the time on the console I see: TcpTimeoutRexmt: Retransmit Timeout. My ftp_server frozen and never becomes alive.

    Regards, Patryk

  • Guru 69970 points

    In reply to Patryk_93:

    Hi,

    Thanks for the update! Not sure if you still in vacation or already back to office. With a small send buffer of 1500 bytes, what is the throughput? Is it satisfactory?

    Regards, Eric

  • In reply to lding:

    Hi,

    Thank you for answer,

    When my buffer is 1500 bytes I have throughput ~2,5MB/s (but transfer is limited by SD card f_read()).

    But when SO_RCVBUF is 32768 transfer transfer is ~5,5 MB/s (f_write()).

    Regards, Patryk

  • Guru 69970 points

    In reply to Patryk_93:

    Hi,

    Theoretically, f_read() is faster than f_write() for a MMCSD card. If your f_write() is 5.5MB/s, what is the f_read() speed standalone (without sending out data to network)? And if you just send a buffer containing garbage data repeatedly using NDK, will SO_SNDBUF >  1500 bytes caused TCP transmit time-out? 

    I want to separate the NDK and MMCSD to understand what the issue on NDK alone with SO_SNDBUF.

    Of course, if you are satisfied with the current throughput, we can close this topic.

    Regards, Eric

  • In reply to lding:

    Hi,

    f_read() speed is more then f_write() and without sending out data to network is more then 10 MB/s.

    Yes, always when I have buffer size more then 1500 bytes it caused TCP transmit time-out..

    MMCSD is insignificant in this case.

    Throughput is too low, because I using FTP to transfer large file.

    Regards, Patryk

  • Guru 69970 points

    In reply to Patryk_93:

    Patryk,

    Thanks! Let me check my colleague in NDK team if they have any suggestions.

    Regards, Eric

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.