Tool/software: TI C/C++ Compiler
Hello,
As mentioned in the latest DM8168 datasheet, DM8168(CYG2) cpu devices speed range is as below :
ARM:1100MHz , DSP:930MHz , HDVICP2:550MHz , SGX530:275MHz ... ... ...
But In my DVRRDK code , ARM_PLL was set to 1.2GHz or 1.0GHz , So we want to set AMR work at the highest speed 1.1GHz.
How to set the paramates in "clocks_ti816x.h" to make A8 work at 1.1GHz ? Is there any tools to caculate these parameters ?
Thanks