Hello
Hopefully someone can point me in the right direction....
I have the AM654x IDK...and I am using the TI-RTOS platform
I am trying to drive one of the LEDS over IC2. Unfortunately I cannot find an example to do this specifically on the AM654x IDK....
Q 1
Is there an example of this using TI-RTOS
Q 2
The device is sold as a SIL 3 device ...IEC51508....etc etc....or should I say it has the possibility of achieving these ratings.
Is there a safety library for this particular device (I believe Hercules has one) and if so, is there a some sort of guide on how to use it with the AM654x
if there is no "safety" library then what is the most recommended library in conjunction with the TI-RTOS platform.
Q 3
Has the device achieved TUV certification or is this still pending.
Kind Regards
Carl