Is it possible to have communication between a Linux Kernel module and a Cortex M4?
Michel Catudal
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it possible to have communication between a Linux Kernel module and a Cortex M4?
Michel Catudal
Hi Michel,
Yes it is possible. You can use IPC via RPMSG protocol.
Linux module is /lib/modules/4.4.84-000340-gaa42c96/kernel/net/rpmsg/rpmsg_proto.ko.
You can refer to API OSA_ipcQueRead() defined in PROCESSOR_SDK_VISION_03_07_00_00\vision_sdk\links_fw\src\hlos\osa\include\osa_ipc_que.h
Regards,
Rishabh
Thank you. that should be helpful.
Is there any TI-RTOS CAN code that uses socket can?
Michel
Hi,
I haven't heard back from you, I'm assuming you were able to resolve your issue.
If not, just post a reply below (or create a new thread if the thread has locked due to time-out).
Regards,
Rishabh