Tool/software: TI C/C++ Compiler
Hi:
We found the DP problem in using EVM boards.
Test environment:
Hardware: AM654X EVM PROCESSOR BOARD (REV 1.0)
TI DP Board( DisplayPort Adapter PROCOO77 REV E1 TC358867)
Monitor:HP-E242 ,HP Compaq LA1951gl
DP-to-VGA adapter's Manufacturer: Choseal, UGREEN, biaze, ce-link
Software: Processor SDK Linux 06_00_00_07 Processor SDK Linux 05_03_00_07
Expected results:
First In the U-boot Setting environment variables :set name_overlays k3-am654-evm-tc358876.dtbo
Using SDK6.0, the EVM board uses the above DP-to-VGA converters to connect the monitor display picture.
Actual results:
Only the UGREEN content DP-to-VGA display has pictures, and ‘Choseal , ce-link, biaze’ has no pictures (these are sure to be all right, verified by PC).
Note: Use our Own board to verify:
1. Using SDK5.3 U-boot can all display pictures (Choseal, UGREEN, ce-link, biaze).
2. Using SDK6.0 U-boot (Keeping the Kernel Mirror Consistent), only UGREEN can display the pictures, which is consistent with the results of the EVM board.
3. So I suspect that it's related to u-boot and I tried to use SDK5.3 on the EVM board to see the phenomenon, but it did not display the picture use all adapters.
SDK5.3 DP erro log:
Tank you for you help!