This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TI-RTOS-PROC: How do I use custom output functions with SysMin?

Expert 5625 points

Replies: 1

Views: 205

Part Number: TI-RTOS-PROC

I have a project that outputs through System_printf() with SysMin, how do I use my own application specific output function?

  • The SysMin module allows users to add their own application specific output function. For example, this can be used to redirect the output to a UART or other peripheral. SysMin buffers data in a circular buffer. When you call System_flush() this data gets pushed to the output function. By default, this output function calls fwrite() (it is actually an internal function used by fwrite in the TI-compiler case) to output the characters to the CIO window in CCS.

    Add this to your .cfg file:

    SysMin = xdc.useModule('xdc.runtime.SysMin');
    System.SupportProxy = SysMin;
    SysMin.outputFxn = "&myOutputFunc";

    And this output function to your .c file. You can replace the call to fwrite() below with a call to the IO operation of your choice.

    #include <stdio.h> // for fwrite()
    
    #include <xdc/std.h>
    #include <xdc/runtime/System.h>
     
    Void myOutputFunc(Char *buf, UInt size)
    {
        fwrite(buf, sizeof(Char), size, stdout);
    }

    The circular buffer is output via the System_flush() API. You can call System_flush() after you call to System_printf() or you can call it in a background thread at lower priority. Note that your output function is called with interrupt disabled so you should be careful with the amount of time that your output function takes.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.