First, I explain my application.
+28V input and converted to +3.3V and +5V.
+3.3V supplies Ethernet-switch-IC and pull-ups for I.MX6.
+5V supplies only USB_OTG/H1_VSUB for i.MX6.
First, +5V enables. Several msec later, +3.3V enables.
I have figures, but I cannot attach it.
Problem:
Any voltage leaks from any voltage source and +3.3V line floats around 0.5V to 1.6V during the period from +5V- enable to +3.3V-enable. On the other hand, our Ethernet-IC can work at Vcc=1.62V, minimum voltage.
Sometimes, Ethernet-IC works abnormally.
My concern and questions:
Enabling +5V before +3.3V-enable causes to float around 0.5V to 1.6V by +5V leaking on the 3.3V line thru any circuit in i.MX 6.
#Do the above phenomena occur in i.MX 6?
#Should +5V enable after 3.3V-enable?