Other Parts Discussed in Thread: OMAPL138,
TI experts,
I am developing a dsp bios project using the latest rtos sdk available for the OMAPL138. My project uses IPC libraries, and initially I wasn't able to compile the project until I added a dummy function for the _mfence function. Once I put that in the main implementation file it compiled no problem. I want to use classes in this project, so I turned on the "Treat C files as C++ files" option in the properties menu, and now the same exact code that was able to compile throws the same error I originally saw when i didn't have the dummy function.
undefined first referenced
symbol in file
--------- ----------------
_mfence
This on a very recent clean install of the latest version of CCS as well.
Thanks,