Part Number: TDA4VMXEVM
Team,
We have a customer trying to evaluate our deep learning library, following this tutorial: They are trying to benchmark this model with TI’s MMA engine. Can you help resolve the error described below?
From the customer: "I am able to convert the model using the TIDL toolchain and run test using the PC emulator.
The problem I met when trying to deploy the model to the board is that after format the SD and put the testvecs folder in, to configure EVM (NO BOOT), and set up CCS, GELS, CCXML. The CCS cannot load the inference binary. Is this the correct instruction to follow in order to test the inference ?
I followed another instruction earlier with the board configured to be SD BOOT MODE with RTOS SDK package and a tidl example included and it was working fine.
I have uploaded our denseline model, test image and config file here."testvecs.zip