Tool/software: TI C/C++ Compiler
Hello,
I was trying to run TIDL segmentation example provided in debian@beaglebone:/usr/share/ti/examples/tidl/segmentation using ./segmentation. but it is raising following error:
debian@beaglebone:/usr/share/ti/examples/tidl/segmentation$ ./segmentation
CMEM Error: init: major version mismatch between interface and driver.
CMEM Error: needs driver version 0x4150002, got 0x4160000
TIOCL FATAL: The cmemk kernel module is not installed. Consult the OpenCL UserGuide at http://software-dl.ti.com/mctools/esd/docs/opencl/index.html
My kernel version is:
4.19.94-ti-r36
I have updated kernel from 4.14. Is that causing problem?
How can I recompile the codes which use TIDL library?
If I try gcc main.cpp in same segmentation folder it raises
debian@beaglebone:/usr/share/ti/examples/tidl/segmentation$ gcc main.cpp
main.cpp:44:22: fatal error: executor.h: No such file or directory
#include "executor.h"
^
compilation terminated.
Also can we use TIDL in python?
Thanks.