This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LINUXEZSDK-DAVINCI: dm365 decoding h264 problem

Part Number: LINUXEZSDK-DAVINCI
Other Parts Discussed in Thread: TMS320DM365

Good day

there is a device, it is known that DaVinci is installed there
 chip encoding "sd" (480p) video and
sending it over ethernet h.264 gdr(Gradual Decoder Refresh)
chip id impossible to see
presumably DM36x
ffmpeg can see the given stream but cannot decode and play it

I understand that there are other sync frames, but we have little time to parse and create a full-fledged program

it is required to capture and decode the stream and then play it on the windows operating system

preferably on ffmpg

there is very little time for work and I would like to receive any ready-made solution even a demo version from old archives
thanks.