Other Parts Discussed in Thread: SYSBIOS
Hi all,
I am trying to attach a JTAG to a DSP while running embedded Linux in the CA15. Apparently there is a conflict between the CA15 and the JTAG, so it won't attach (JTAG is working OK bare metal).
The details of the HW and SW are:
Target board: DRA7x EVM
JTAG: Lauterbach Power Debug Pro
OS: Arago (Processor SDK 06.01.00.08)
kernel: 4.19.59
Any hint regarding this issue? Is module remoteproc conflicting the JTAG connection? If this is the case, is there any configuration/setting that can allow to connect to the DSP for debugging?
Thanks in advance,