Hi Team,
Shall I use USB3.1 (Gen1/Gen2) compliant ESD/TVS diodes for USB2.0 application?
If I can use, what are all the parameters I need to check?
Regards,
Santhana Krishnan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Shall I use USB3.1 (Gen1/Gen2) compliant ESD/TVS diodes for USB2.0 application?
If I can use, what are all the parameters I need to check?
Regards,
Santhana Krishnan
Hi Santhana,
Welcome to E2E!
For USB3.1 applications the capacitance of the device is very important to not affect signal integrity of the high speed interface. The data speeds in USB2.0 are much slower so the same device can be used. A device with a higher capacitance could also be used if beneficial to the system(e.g. higher ESD protection, price, etc.)
Key parameters to check in a system would be the reverse stand off voltage (or working voltage), the IEC 61000-4-2 ESD protection capabilities of the device, the clamping voltage of the device, and the capacitance.
Here is the link to a short series of training videos on ESD essentials if you would like to learn more: ESD Essentials
Best regards,
Andy Robles