This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CC1312R IF frequency

What the IF frequency at CC1312R? same as at CC1310 IF=250MHz?

I need it for image rejection test.

Regards,

  • Expert 7615 points
    Hello,

    IF frequency is a function on receiver bandwidth setting. What setting are you using?

    Regards,

    SVS

  • In reply to SVS:

    receiver bandwidth 118 KHz

  • In reply to Michael Ishakbaev:

    118KHz
  • In reply to SVS:

    118KHz

  • Expert 7615 points

    In reply to Michael Ishakbaev:

    Yes, the IF is 250KHz at this RX BW setting on CC1312 as well.

    Regards,

    SVS

  • In reply to SVS:

    Ok, thank you.

    i have EVB 1312R1,imaje rejection(-500kHz offset from wanted signal) is ~27dB.

    set up is : -95dBm wanted signal,  RX BW=118KHz.

  • In reply to Michael Ishakbaev:

    The default IF frequency is found in the user guide on page 2029.

    www.ti.com/.../swcu185a.pdf

    It also includes a small discussion about how to override the default values.

    Regards,
    /TA

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer
     button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

  • In reply to TA12012:

    how i can canceled the imaje by some command rf studio?
  • Expert 7615 points

    In reply to Michael Ishakbaev:

    Are you looking for image rejection performance on the device?

    SVS

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.