This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ADC32RF80: Hardware reset of Power-Up Sequence

Expert 1500 points

Replies: 2

Views: 649

Part Number: ADC32RF80

Hello,

I have a question about Hardware reset of ADC32RF80.

[Q]

The figure below is the sequence described on D/S.
I have a question about Hardware reset in Step 3.

Hardware reset is RESET pin (48).
In Step 3 in the Start-Up Sequence, it is said that hardware reset is applied at pins 33 and 34.
Pin 33 and pin 34 are SYSREFP / M.
Is this a pin 48 mistake? Or is it correct?

Best Regards,

Kaede Kudo

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.