This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Using CC2590 to boost CC2640 output

Prodigy 110 points

Replies: 3

Views: 811

Hi, I am looking for some design guide or reference design for adding the CC2590 booster to the RF outputs of the CC2640. I need to boost the +5dBm output from the CC2640 up to +14dBm that the CC2590 provides. There are reference designs for CC25xx and CC24xx devices but nothing for the CC2640.

I am also interested to know if I should supply CC2590 Vdd with the DCDC Vdds output from the CC2640 or from the independent 3.3V power supply. Any help would be appreciated.

Cheers,

Phil.

  • Expert 6695 points
    Dear Phil,

    Please take a look at this reference design:
    www.ti.com/.../TIDC-CC2650-CC2592-EMK

    You can also take a look at these E2E threads:
    e2e.ti.com/.../590465
    e2e.ti.com/.../499049

    Best Regards,
    R.M
  • In reply to R.M:

    Thanks R.M, this is helpful. Can you let me know how the L3 between RF_P and RF_N should have its value determined? 

    Cheers,

    Phil.

  • Expert 6695 points

    In reply to Philip Craig:

    Hi Phil,

    L3 is not mounted by default but it's recommended to have a footprint for a component there if tuning becomes needed on your custom design.

    Best Regards,
    Reidar

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.