This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

AFE7686: AFE7686 direct connection to 66AK2K2L device

Prodigy 240 points

Replies: 5

Views: 1281

Part Number: AFE7686

Can I interface the AFE7686 directly to the 66AK2K2L chip using just 2 JESD204 lanes for xmit and rcv?  Also, can I operate the AFE7686 ADC in the second nyquist zone (subsampling 1.5-3GHz)?

  • Hi DocT

    Can you provide information on the bandwidths you like to support on the xmit and rcv?
    Yes, 2nd Nyquist operation for the receiver is possible.

    Thanks,
    Eben.
  • In reply to Ebenezer Dwobeng:

    Maximum of 200 MHz rx bandwidth before digital tuning. tx bandwidth 10 MHz max
  • In reply to DocT:

    Hi DocT,

    This should be possible for 1T1R configuration with a data rate of 245.76MHz for both TX and RX and JESD mode of L-M-F-S-Hd=2-2-2-1-0.
    Because this device is 4T4R, can you also consider using discrete devices like DAC38RF8x and ADC32RF45?

    Thanks,
    Eben.
  • In reply to Ebenezer Dwobeng:

    Yes I can but I have space an power constraints.  My thought was the AFExxxx front end chips would reduce the amount of PCB area needed.  What is the advantage of going with discrete devices?

  • In reply to DocT:

    Hi DocT,

    You are right about the savings in area.
    My only concern with the AFExxx for 1T1R application was that you will not be utilizing all the DAC and ADC cores available in the device and so it may not be the most efficient solution.

    Thanks,
    Eben.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.