This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CC1200 & 5.9 GHz RF

Intellectual 890 points

Replies: 4

Views: 970

Hi,

We have used CC1200 to communicate between 2 platforms. Now we need to replace that communication with other system that communicates at 5.9GHz. We could not find an IC from TI that can achieve that in a simple way as CC1200 achieves the sub-GHz communication.

Are we correct?...TI does not  provide any solution for communication at 5.9GHz?

Regards

Sam

  • Guru 221765 points
    Not that I'm aware of. Which standard uses 5.9 GHz?

     

  • In reply to TER:

    V2V and DSRC to name two
  • In reply to TER:

    V2V....DSRC standards do use 5.9GHz


    does TI have an IC that allows us to create arbitrary carrier frequency?
  • Guru 221765 points

    In reply to Sam Ref:

    The closest I could find here is: www.ti.com/.../overview.html

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.