This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Output frequency LMX2582, TICS pro

Prodigy 130 points

Replies: 1

Views: 291

i

I have a question about configuring LMX2582.
The chip is palced on the evaluation board ADC32RF80EVM and I try to get 3GHz from LMX2582 outputs.
His input frequency = 122.88MHz (get from LMK04828).
I used "Tics pro" and set such values:
Input chain: Doubler = x1, Pre-R=1, Multiplier=1, Post-R=1.
Feedback: Prescaler = 2, Ndivider = 24, Fnum = 53, Fden = 128.
F_VCO = 6000 MGz.
Outputs chain: SEG1 = /2, Channel Divider MUX = SEG1, Output MUX = CHDIV.
So RFOutA = 3000MHz.
BUT: instead of 3000M, RFOutA is about 3031M.
I attached file *.tcs for "TICS Pro", may be you can help me to set right registers values?(I changed extension as  the site refuse to attach *.tcs)

Thanks.

5100.ADC_evm_3000p00_4xIQ_8411_.cfglmx_TI_TCS.txt

  • Nick,

    I looked at the fine and nothing seems wrong about the frequencies. You should change OUTx_PWR, but this would not cause your issue. I do wonder if this is related to the VCO calibration. I would try changing CAL_CLK_DIV from divide by 1 to divide by 8 to see if it is related to this.

    The VCO divides the frequency into 6 VCO cores and each core has 183 different bands. So if the VCO calibration gets off, that would be an issue.

    Regards,
    Dean

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.