This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ADS58J89EVM: Sampling with HSDCPro Automation DLL

Prodigy 10 points

Replies: 1

Views: 216

Part Number: ADS58J89EVM

Hello,

we have got a ADS58J89EVM and TSW14J56 hooked up for sampling. Also, we are using HSDCPro Automation DLL for sampling with MATLAB. I got a couple of questions.

1- What is the output unit of sampled data saved in the CSV file? is it mv?

2- How can we sample continuously? It looks like after each run of MATLAB codes, it takes samples only once.

3- It takes about 2.5s to sample with fs=125MHz and No. of samples=65536. How can I make it faster?

Thanks

  • Hi Dave,

    1-The output is raw ADC codes in 14bits resolution. It is unit-less. To convert to mV, divide the code by full scale code (=2^13-1) and multiply by the full scale amplitude. Full scale amplitude is 625mV by default
    2-Continuous capture is not supported in the automation functions. You can enable continuous capture manually from data capture options menu in HSDCPRO
    3-There is no way to speed up the capture.

    Thanks,
    Eben.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.