This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TRF372017: What's the baseband input range?

Prodigy 10 points

Replies: 1

Views: 104

Part Number: TRF372017

I find there is no description about the input Peak-Peak range.

Plz ,help me to find it

  • The nominal input swing to the I/Q ports is differential 1V peak-to-peak.  You can check out Figure 1 in the TRF370317 datasheet which depicts the power output with respect to input swing (SE in the graph).  The modulator portion of the TRF3702017 shares the same IP as the TRF370317. 

    --RJH

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.