• Resolved

IWR1443BOOST

Prodigy 90 points

Replies: 8

Views: 143

Hi,

      Write IWR1443 appear "Image load failed: !!! Aborting of specified files !!!".please help.

Thank!

  • Hi User,

    Where are you seeing this error? Would you be able to post a screenshot?

    We'll require more information in order to assist you.

    Cheers,

    Akash

  • In reply to Akash Gondalia:

      

  • In reply to user5233161:

     使用的是 IWR1443 ES 03.0.0

  • In reply to user5233161:

    Hi User,

    The High Accuracy 14xx Lab in the Industrial Toolbox 4.0.1 is for ES2.0 but we will be releasing an update to this software which is compatible with ES3.0 in early November. It will be part of the Industrial Toolbox 4.1.0.

    Cheers,

    Akash

  • In reply to Akash Gondalia:

    Hi Akash,

    Looking forward to an early release.

    Thank!

    yipeng

  • In reply to user5233161:

    Hi Akash,

    Have you released the update? I think I have the same problem.

    Thanks

    Gio

  • In reply to Giovanni Campanella:

    Hi Gio,

    It will be available on TIREX as part of the Industrial Toolbox version 4.1.0. It will probably go live on Monday.

    Cheers,

    Akash

  • In reply to Akash Gondalia:

    Hi Akash,

    Thanks for replying and looking forward to the update release. Just as a side note I think it creates a bit of confusion not having on the web the most up to date software that runs on the latest hardware release. 

    Hope this can be improved in future.

    Thanks

    Giovanni