Hello,
I have a question about Hardware reset of ADC32RF80.
[Q]
The figure below is the sequence described on D/S.
I have a question about Hardware reset in Step 3.
Hardware reset is RESET pin (48).
In Step 3 in the Start-Up Sequence, it is said that hardware reset is applied at pins 33 and 34.
Pin 33 and pin 34 are SYSREFP / M.
Is this a pin 48 mistake? Or is it correct?
Best Regards,
Kaede Kudo