This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LM15851EVM: the LM15851 placement

Intellectual 670 points

Replies: 2

Views: 677

Part Number: LM15851EVM

Hi!

Can you tell me please, why did you place the LM15851 on the opposite side of the board?

Thanks in advance!

Best regards, Vic.

  • Hi Vic
    This was done to provide the best routing from the LM15851 JESD204B data output terminals to the matching signal locations on the FMC connector.
    If the LM15851 is on the top side of the board all of the signal pairs need to cross over each-other. This causes more complex signal routing, adding vias etc. which could potentially degrade the high speed serial data signals.
    Best regards,
    Jim B
  • In reply to Jim Brinkhurst84999:

    Thanks a lot, Jim, for the fast reply!
    Best regards,
    Vic.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.