Hello guys!
I have a curiosity regarding the components that precede the antenna in the CC2540 microcontroller according to the figure, can someone explain to me why it has to use that part?
Obs, I'm using the 2.4GHz design (AN043)
Taking advantage of the post, I would also like to know the summarized function of the two crystals present in the typical application (32 MHz and 32 kHz), read something on a frequency of 16 MHz also, this frequency of 16 MHz is an internal oscillator of the CC2540?
Thanks in advance and sorry if it was stupid questions.