This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ADC32RF80: ADC32RF80

Prodigy 130 points

Replies: 1

Views: 719

Part Number: ADC32RF80

Hi

In the datasheet for ADC32RF80 all calculations and graphs was made for Fs = 2949.12M. But description on your site say Fs_max = 3000M, so Fs can be 3000M. On the other hand, the built-in NCO has resolution 16 bits, (2^16 = 65366), thus his freq step is 2949.12M/2^16 = 45000 Hz or 3000M/2^16 = 45776,3671875 Hz. The second version is not good. That's why there is on the evaluation board the crystal oscillator with frequency =  122.88M (122.88M*24 = 2949.12M).

But ADC itself CAN work on sampling frequency =  3000M. Do I understand this correctly?

Thank you. 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.