This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 5
Views: 359
HELLO'
I HAVE A PROBLEM TO CONECT THE WATCH TO THE PC WITh THE RF
can it be that the emulator dosnet work with windows 10?
In reply to R.M:
I can't connect to a pc. It doesn't even matter if I start the accesspoint on the pc or not. The chronos always crashes when I try to start the connection, this is for all types, acc, ppt and sync. after the crash/restart, the watch is back at 4:30 and the complete LCD screen is on
In reply to vadim roizman:
Dear Vadim, I see that you are getting help on this in a different E2E thread (link). I will close this thread, please post any additional question there and they will try to help you. Best Regards, R.M