This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Need Voltage Feedback or Current Feedback op-amp suitable for use at 1GHz and above

Intellectual 350 points

Replies: 2

Views: 228

Need Voltage Feedback or Current Feedback op-amp suitable for use at 1GHz and above 

The application is a standard summing amplifier where multiple inputs are applied to the virtual ground inverting input.

  • Hello Arthur,

    I see that you already have a thread open with the same question. I am going to close this thread and assist you on that thread. Sorry for the delayed response.

    Thanks!
    -Karan
  • In reply to Karan Kotadia:

    still need an amplifier suitable for use as a summing amplifier up to 1 GHz

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.