This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TSW40RF80EVM: TSW40RF80EVM need US re-export licence required?

Prodigy 220 points

Replies: 1

Views: 210

Part Number: TSW40RF80EVM

Device TSW40RF80EVM need US re-export license required?

If the parameters shown below are met or exceeded for the part TSW40RF80EVM

if US re-export license is required pls support written/email confirmation

3A101.a.2.b. Electrical input type analog-to-digital converter printed circuit boards or modules, having all of the following characteristics:

a.2.b.1. Rated for operation in the temperature range from below -45°C to above +80°C; and

a.2.b.2. Incorporating microcircuits identified in 3A101.a.2 .a;

 

3A101.a.2 .a;. Analog-to-digital converter microcircuits which are radiation-hardened or have all of the following characteristics:

a.2.a.1. Rated for operation in the temperature range from below -54°C to above +125°C; and

a.2.a.2. Hermetically sealed;

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.