This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TSW40RF80EVM: Request TI to confirm if TSW40RF80EVM meet or exceed the followings

Prodigy 220 points

Replies: 1

Views: 203

Part Number: TSW40RF80EVM

Solved ECCN # to 3A002 from ECCN team

But Avnet EUS team still request  as below it

Pls confirm this.

TSW40RF80EVM

MT applies to 3A002.h when the parameters in 3A101.a.2.b are met or exceeded

3A101.a.2.b. Electrical input type analog-to-digital converter printed circuit boards or modules, having all of the following characteristics:

a.2.b.1. Rated for operation in the temperature range from below -45°C to above +80°C; and

a.2.b.2. Incorporating microcircuits identified in 3A101.a.2 .a;

 

3A101.a.2 .a;. Analog-to-digital converter microcircuits which are radiation-hardened or have all of the following characteristics:

a.2.a.1. Rated for operation in the temperature range from below -54°C to above +125°C; and

a.2.a.2. Hermetically sealed;

  • I am not sure that I follow the question. The TSW40RF80 is a reference design that incorporates the DAC38RF80 and ADC32RF45 RF sampling converters. Perhaps the question is really related to the classification of those particular devices. Those devices operating temp range is -40 degC to +85 degC; they are not intended for Rad-Hard applications.

    --RJH

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.