Hello.
Is it possible for AWR1843 chip to create more than 4 profiles?
To increase the number of profiles, I changed the constants MMWAVE_MAX_PROFILE and RL_MAX_PROFILES_CNT, but the rlSetProfileConfig function returns an error code (#35. AWR_PROFILE_CONF_SET_SB, “PF_INDX is≥4”).
Is there a possible to support more than 4 profiles in the BSS domain?