Other Parts Discussed in Thread: DAC38RF82
Hello RF Team,
Regarding TRF370417
The datasheet mentioned that this part supports an I/Q baseband input bandwidth of 1-GHz. With this bandwidth capability the input signal can be centered at a high IF frequency to provide frequency separation from unwanted carrier feed-through or sideband image. Utilizing the full baseband bandwidth yields an RF output bandwidth up to 2-GHz
What is 3dB Bandwidth ? (is it 1GHz ? or Higher )
Do you have graph of the Baseband I/Q Bandwidth ?
Many thanks in advance,
Doron